CylinderMillingCutParametersCutDirectionTypes Enumeration

NXOpen.CAM.CylinderMillingCutParameters.CutDirectionTypes is an alias for NXOpen.CAM.CylinderMillingCutParametersCutDirectionTypes

class NXOpen.CAM.CylinderMillingCutParametersCutDirectionTypes

Bases: object

cut direction options

New in version NX8.0.0.

Enum Members

Enum Member Enum Member Description
Climb
Climb cut
Conventional
Conventional cut
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.