CylindricalMillingCutParameters Class

class NXOpen.CAM.CylindricalMillingCutParameters

Bases: NXOpen.CAM.FeatureMillingCutParameters

Represents a CylindricalMillingCutParameters Builder

This is an abstract class and cannot be instantiated.

New in version NX9.0.2.

Properties

Property Description
BottomOffset Returns the bottom offset
BottomStock Returns the bottom stock
CheckIpwCollisions Returns or sets the value to Check for Ipw Collsions
CheckSafeClearance Returns the Check Safe Clearance
ContinuousCut Returns or sets the continuous cut
CuttingDirection Returns or sets the cut direction
HolderClearance Returns the Holder Clearance
IpwType Returns or sets the IPW type
NeckClearance Returns the Neck Clearance
PartSafeClearance Returns the Part Safe Clearance
PartStock Returns the part stock
ShankClearance Returns the Shank Clearance
Tag Returns the Tag for this object.
Tolerances Returns the Tolerances builder
TopOffset Returns the top offset
UseToolHolder Returns or sets the use tool holder

Methods

Property Detail

BottomOffset

CylindricalMillingCutParameters.BottomOffset

Returns the bottom offset

-------------------------------------

Getter Method

Signature BottomOffset()

Returns:the bottom offset builder
Return type:NXOpen.CAM.VerticalPosition

New in version NX9.0.2.

License requirements: None.

ContinuousCut

CylindricalMillingCutParameters.ContinuousCut

Returns or sets the continuous cut

-------------------------------------

Getter Method

Signature ContinuousCut()

Returns:the continuous cut
Return type:bool

New in version NX9.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature ContinuousCut(continuousCut)

Parameters:continuousCut (bool) – the continuous cut

New in version NX9.0.2.

License requirements: cam_base (“CAM BASE”)