CylinderMillingBuilderBlankDiameterTypes Enumeration

NXOpen.CAM.CylinderMillingBuilder.BlankDiameterTypes is an alias for NXOpen.CAM.CylinderMillingBuilderBlankDiameterTypes

class NXOpen.CAM.CylinderMillingBuilderBlankDiameterTypes

Bases: object

blank diamter options

New in version NX8.0.0.

Enum Members

Enum Member Enum Member Description
Diameter
Diameter
Distance
distance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.