CylinderMillingBuilderDepthPerRevolutionTypes Enumeration

NXOpen.CAM.CylinderMillingBuilder.DepthPerRevolutionTypes is an alias for NXOpen.CAM.CylinderMillingBuilderDepthPerRevolutionTypes

class NXOpen.CAM.CylinderMillingBuilderDepthPerRevolutionTypes

Bases: object

Depth Per Revolution options

New in version NX8.0.0.

Enum Members

Enum Member Enum Member Description
Distance
Distance
RampAngle
Ramp Angle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.