CylinderMillingBuilderDiameterForHelixTypes Enumeration

NXOpen.CAM.CylinderMillingBuilder.DiameterForHelixTypes is an alias for NXOpen.CAM.CylinderMillingBuilderDiameterForHelixTypes

class NXOpen.CAM.CylinderMillingBuilderDiameterForHelixTypes

Bases: object

Diameter for Helix

New in version NX8.0.0.

Enum Members

Enum Member Enum Member Description
Diameter
Helix Diameter
SpiralThickness
Spiral Thickness
OffsetFromStartDiameter
Offset from Start Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.