ModalResultsEvaluationSettingBuilder Class

class NXOpen.CAE.ResponseSimulation.ModalResultsEvaluationSettingBuilder

Bases: NXOpen.CAE.ResponseSimulation.FunctionEvaluationSettingBuilder

Represents the abstract builder class of evaluation setting for FRF and transmissibility

This is an abstract class, and cannot be created.

New in version NX5.0.0.

Properties

Property Description
DataLocation Returns the frequency setting
EvaluationProperty Returns the frequency setting
InputDirection Returns or sets the source direction data component
InputNode Returns or sets the source node.
ObservationNode Returns or sets the observation nodes.
OutputRequest Returns or sets the destination direction data component
OutputSettings Returns the output setting.
ResultType Returns or sets the result type
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
GetOutputElements Returns destination nodes.
GetOutputNodes Returns destination nodes.
SetOutputElements Sets destination nodes
SetOutputNodes Sets destination nodes
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

DataLocation

ModalResultsEvaluationSettingBuilder.DataLocation

Returns the frequency setting

-------------------------------------

Getter Method

Signature DataLocation()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.DataLocation

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

EvaluationProperty

ModalResultsEvaluationSettingBuilder.EvaluationProperty

Returns the frequency setting

-------------------------------------

Getter Method

Signature EvaluationProperty()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.FrequencyDefinition

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

InputDirection

ModalResultsEvaluationSettingBuilder.InputDirection

Returns or sets the source direction data component

-------------------------------------

Getter Method

Signature InputDirection()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.DirectionDataComponent

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature InputDirection(dataComponent)

Parameters:dataComponent (NXOpen.CAE.ResponseSimulation.DirectionDataComponent) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

InputNode

ModalResultsEvaluationSettingBuilder.InputNode

Returns or sets the source node.

-------------------------------------

Getter Method

Signature InputNode()

Returns:
Return type:NXOpen.CAE.FENode

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature InputNode(sourceNode)

Parameters:sourceNode (NXOpen.CAE.FENode) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

ObservationNode

ModalResultsEvaluationSettingBuilder.ObservationNode

Returns or sets the observation nodes.

-------------------------------------

Getter Method

Signature ObservationNode()

Returns:
Return type:NXOpen.CAE.FENode

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature ObservationNode(observationNode)

Parameters:observationNode (NXOpen.CAE.FENode) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

OutputRequest

ModalResultsEvaluationSettingBuilder.OutputRequest

Returns or sets the destination direction data component

-------------------------------------

Getter Method

Signature OutputRequest()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.DirectionDataComponent

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature OutputRequest(dataComponent)

Parameters:dataComponent (NXOpen.CAE.ResponseSimulation.DirectionDataComponent) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Method Detail

GetOutputElements

ModalResultsEvaluationSettingBuilder.GetOutputElements

Returns destination nodes.

Only available when result type is CAE.ResponseSimulationEvaluationResultType.Stress, CAE.ResponseSimulationEvaluationResultType.Strain, CAE.ResponseSimulationEvaluationResultType.ShellStressResultant

Signature GetOutputElements()

Returns:
Return type:list of NXOpen.CAE.FEElement

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

GetOutputNodes

ModalResultsEvaluationSettingBuilder.GetOutputNodes

Returns destination nodes.

Only available when result type is CAE.ResponseSimulationEvaluationResultType.Displacement, CAE.ResponseSimulationEvaluationResultType.Velocity, CAE.ResponseSimulationEvaluationResultType.Acceleration, CAE.ResponseSimulationEvaluationResultType.ReactionForce

Signature GetOutputNodes()

Returns:
Return type:list of NXOpen.CAE.FENode

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

SetOutputElements

ModalResultsEvaluationSettingBuilder.SetOutputElements

Sets destination nodes

Signature SetOutputElements(destinationElements)

Parameters:destinationElements (list of NXOpen.CAE.FEElement) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

SetOutputNodes

ModalResultsEvaluationSettingBuilder.SetOutputNodes

Sets destination nodes

Signature SetOutputNodes(destinationNode)

Parameters:destinationNode (list of NXOpen.CAE.FENode) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Validate

ModalResultsEvaluationSettingBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.