DataLocation Class¶
-
class
NXOpen.CAE.ResponseSimulation.
DataLocation
¶ Bases:
NXOpen.TaggedObject
Represents the data location to perform evaluation
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BeamLocation | Returns or sets the method to define frequency |
ElementLocation | Returns or sets the element location. |
LayerSelection | Returns or sets the end value of frequency range. |
ShellLocation | Returns or sets the start value of frequency range. |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
DataLocationBeam Enumeration | Specifies the location for beam |
DataLocationElement Enumeration | Specifies the element location for element |
DataLocationShell Enumeration | Specifies the location for shell |
Property Detail¶
BeamLocation¶
-
DataLocation.
BeamLocation
¶ Returns or sets the method to define frequency
-------------------------------------
Getter Method
Signature
BeamLocation()
Returns: Return type: NXOpen.CAE.ResponseSimulation.DataLocationBeam
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
BeamLocation(beamLocation)
Parameters: beamLocation ( NXOpen.CAE.ResponseSimulation.DataLocationBeam
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ElementLocation¶
-
DataLocation.
ElementLocation
¶ Returns or sets the element location.
Only available when stress and strain is defined by
CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range
-------------------------------------
Getter Method
Signature
ElementLocation()
Returns: Return type: NXOpen.CAE.ResponseSimulation.DataLocationElement
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ElementLocation(elementLocation)
Parameters: elementLocation ( NXOpen.CAE.ResponseSimulation.DataLocationElement
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
LayerSelection¶
-
DataLocation.
LayerSelection
¶ Returns or sets the end value of frequency range.
Only available when the frequency is defined by
CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range
-------------------------------------
Getter Method
Signature
LayerSelection()
Returns: Return type: int New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
LayerSelection(layerNumber)
Parameters: layerNumber (int) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ShellLocation¶
-
DataLocation.
ShellLocation
¶ Returns or sets the start value of frequency range.
Only available when the frequency is defined by
CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range
-------------------------------------
Getter Method
Signature
ShellLocation()
Returns: Return type: NXOpen.CAE.ResponseSimulation.DataLocationShell
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ShellLocation(shellLocation)
Parameters: shellLocation ( NXOpen.CAE.ResponseSimulation.DataLocationShell
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)