FunctionEvaluationSettingBuilder Class

class NXOpen.CAE.ResponseSimulation.FunctionEvaluationSettingBuilder

Bases: NXOpen.Builder

Represents the abstract builder class of evaluation setting for function response evaluation

This is an abstract class, and cannot be created.

New in version NX5.0.0.

Properties

Property Description
OutputSettings Returns the output setting.
ResultType Returns or sets the result type
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

OutputSettings

FunctionEvaluationSettingBuilder.OutputSettings

Returns the output setting.

-------------------------------------

Getter Method

Signature OutputSettings()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.FunctionEvaluationOutputSettings

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

ResultType

FunctionEvaluationSettingBuilder.ResultType

Returns or sets the result type

-------------------------------------

Getter Method

Signature ResultType()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.EvaluationResultType

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature ResultType(resultType)

Parameters:resultType (NXOpen.CAE.ResponseSimulation.EvaluationResultType) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Method Detail

Validate

FunctionEvaluationSettingBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.