FunctionEvaluationOutputSettings Class¶
-
class
NXOpen.CAE.ResponseSimulation.
FunctionEvaluationOutputSettings
¶ Bases:
NXOpen.TaggedObject
Represents the output setting for function response evaluation
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
RecordPrefix | Returns or sets the prefix of evaluation results record name |
ShowPlot | Returns or sets the option of show plot. |
StoreOption | Returns or sets the store option. |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
RecordPrefix¶
-
FunctionEvaluationOutputSettings.
RecordPrefix
¶ Returns or sets the prefix of evaluation results record name
-------------------------------------
Getter Method
Signature
RecordPrefix()
Returns: Return type: str New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
RecordPrefix(recordPrefix)
Parameters: recordPrefix (str) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ShowPlot¶
-
FunctionEvaluationOutputSettings.
ShowPlot
¶ Returns or sets the option of show plot.
If true, the evaluation results will be displayed on screen
-------------------------------------
Getter Method
Signature
ShowPlot()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ShowPlot(showPlot)
Parameters: showPlot (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
StoreOption¶
-
FunctionEvaluationOutputSettings.
StoreOption
¶ Returns or sets the store option.
If true, the evaluation results will be stored on disk
-------------------------------------
Getter Method
Signature
StoreOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
StoreOption(storeOption)
Parameters: storeOption (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)