FrequencyDefinition Class

class NXOpen.CAE.ResponseSimulation.FrequencyDefinition

Bases: NXOpen.TaggedObject

Represents the frequency setting to perform FRF evaluation

New in version NX5.0.0.

Properties

Property Description
ContributorNumber Returns or sets the number of contributors.
EndValue Returns or sets the end value of frequency range.
EvaluationType Returns or sets the method to define frequency
GenerateMaximumContributors Returns or sets the option for generating maximum contributors or not.
InterpolationMethodOption Returns or sets the interpolation method.
NormalizeResults Returns or sets the option to normalize results.
SpectralLine Returns or sets the additional spectral lines.
StartValue Returns or sets the start value of frequency range.
Tag Returns the Tag for this object.

Methods

Method Description
GetFrequencies Returns frequency values to perform FRF evaluation.
SetFrequencies Sets the frequency values to perform FRF evaluation.

Enumerations

FrequencyDefinitionDefinition Enumeration Specifies the method to define frequency
FrequencyDefinitionInterpolationMethod Enumeration Specifies the method for interpolation

Property Detail

ContributorNumber

FrequencyDefinition.ContributorNumber

Returns or sets the number of contributors.

Only available when maximu contributors will be generated

-------------------------------------

Getter Method

Signature ContributorNumber()

Returns:
Return type:int

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature ContributorNumber(contributorNumber)

Parameters:contributorNumber (int) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

EndValue

FrequencyDefinition.EndValue

Returns or sets the end value of frequency range.

Only available when the frequency is defined by CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range

-------------------------------------

Getter Method

Signature EndValue()

Returns:
Return type:float

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature EndValue(endValue)

Parameters:endValue (float) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

EvaluationType

FrequencyDefinition.EvaluationType

Returns or sets the method to define frequency

-------------------------------------

Getter Method

Signature EvaluationType()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.FrequencyDefinitionDefinition

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature EvaluationType(type)

Parameters:type (NXOpen.CAE.ResponseSimulation.FrequencyDefinitionDefinition) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

GenerateMaximumContributors

FrequencyDefinition.GenerateMaximumContributors

Returns or sets the option for generating maximum contributors or not.

Only available when frequency definition metod is CAE.ResponseSimulation.FrequencyDefinitionDefinition.ModalContribution

-------------------------------------

Getter Method

Signature GenerateMaximumContributors()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature GenerateMaximumContributors(generateMaximumContributors)

Parameters:generateMaximumContributors (bool) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

InterpolationMethodOption

FrequencyDefinition.InterpolationMethodOption

Returns or sets the interpolation method.

Only available when the frequency is defined by CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range

-------------------------------------

Getter Method

Signature InterpolationMethodOption()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.FrequencyDefinitionInterpolationMethod

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature InterpolationMethodOption(interpolationMethod)

Parameters:interpolationMethod (NXOpen.CAE.ResponseSimulation.FrequencyDefinitionInterpolationMethod) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

NormalizeResults

FrequencyDefinition.NormalizeResults

Returns or sets the option to normalize results.

Only available when maximu contributors will be generated

-------------------------------------

Getter Method

Signature NormalizeResults()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature NormalizeResults(normalizeResults)

Parameters:normalizeResults (bool) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

SpectralLine

FrequencyDefinition.SpectralLine

Returns or sets the additional spectral lines.

Only available when frequency is defined by CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range

-------------------------------------

Getter Method

Signature SpectralLine()

Returns:
Return type:int

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature SpectralLine(spectralLines)

Parameters:spectralLines (int) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

StartValue

FrequencyDefinition.StartValue

Returns or sets the start value of frequency range.

Only available when the frequency is defined by CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range

-------------------------------------

Getter Method

Signature StartValue()

Returns:
Return type:float

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature StartValue(startValue)

Parameters:startValue (float) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Method Detail

GetFrequencies

FrequencyDefinition.GetFrequencies

Returns frequency values to perform FRF evaluation.

Only available when the frequency definition method is CAE.ResponseSimulation.FrequencyDefinitionDefinition.ModalContribution

Signature GetFrequencies()

Returns:
Return type:list of float

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

SetFrequencies

FrequencyDefinition.SetFrequencies

Sets the frequency values to perform FRF evaluation.

Only available when the frequency definition method is CAE.ResponseSimulation.FrequencyDefinitionDefinition.ModalContribution

Signature SetFrequencies(frequencies)

Parameters:frequencies (list of float) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)