FrequencyDefinitionInterpolationMethod Enumeration

NXOpen.CAE.ResponseSimulation.FrequencyDefinition.InterpolationMethod is an alias for NXOpen.CAE.ResponseSimulation.FrequencyDefinitionInterpolationMethod

class NXOpen.CAE.ResponseSimulation.FrequencyDefinitionInterpolationMethod

Bases: object

Specifies the method for interpolation

Enum Members

Enum Member Enum Member Description
LogLog  
LogLinear  
LinearLinear  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.