Selection Class¶
Methods¶
Method | Description |
---|---|
AddToSelectionList | Add objects to the selection list. |
AddToTaggedObjectsSelectionList | Add objects to the selection list. |
AskSelectionCursorPosition | Returns the view and absolute coordinates of the cursor position for the associated selection. |
AskSelectionDescriptor | Returns the information in SelectionSelectionDescriptor_Struct describing the selection that was just performed. |
AskSelectionListCount | Returns the number of objects currently selected. |
AskSelectionObjectList | Returns the number of objects selected and a pointer to an array of tags of the objects selected. |
AskSelectionRectanglePosition | Returns the absolute coordinates of the rectangle cursor positions. |
AskSelectionTaggedObjectList | Returns the number of tagged objects selected and a pointer to an array of tags of the objects selected. |
GetNumSelectedObjects | Returns the number of objects currently selected @return The number of objects currently selected |
GetSelectedObject | Returns the n’th object on the selection list @return The object at the given position on the selection list. |
GetSelectedTaggedObject | Returns the n’th tagged object on the selection list @return The object at the given position on the selection list. |
GetSelectionStatusOfUserDefinedClass | Gets whether or not the user defined class is available for selection. |
IsObjectInSelectionList | Inquires if object is selected. |
RemoveAllFromSelectionList | Removes all the objects from the selection list and optionally unhighlights them. |
RemoveFromSelectionList | Removes objects from the selection list. |
RemoveTaggedObjectsFromSelectionList | Removes tagged objects from the selection list. |
SelectFeatures | Select features @return Ok, Back, or Cancel |
SelectObject | Select single object. |
SelectObjects | Select objects. |
SelectScreenPosition | Select screen position on graphics display @return Pick, Back, or Cancel |
SelectTaggedObject | Select single tagged object. |
SelectTaggedObjects | Select tagged objects. |
SetSelectType | Sets the selection type. |
SetSelectionCallbacks | Specify selection filter callback for additional filtering based on application specific criteria, and/or selection callback to perform application specific processing for each selection gesture processed. |
SetSelectionMask | Sets the types of objects that are selectable. |
SetSelectionStatusOfUserDefinedClass | Sets whether or not the user defined class is available for selection. |
SetTaggedObjectSelectionCallbacks | Specify selection filter callback for additional filtering of tagged objects based on application specific criteria, and/or selection callback to perform application specific processing for each selection gesture processed. |
Enumerations¶
SelectionDialogResponse Enumeration | Specify the user response for general dialogs. |
SelectionResponse Enumeration | Specify the user response for the selection operation. |
SelectionSelectionAction Enumeration | Indicates the type of action to perform when an object is selected. |
SelectionSelectionFeatureType Enumeration | Specify the type of features to select. |
SelectionSelectionScope Enumeration | Indicates the scope for selecting objects. |
SelectionSelectionType Enumeration | Indicates the general class of object to filter selection. |
SelectionUistylerSelectionType Enumeration | Indicates the general class of object to filter selection. |
Structs¶
SelectionMaskTriple_Struct Struct | Used in selection methods to set the types of objects that are selectable. |
SelectionSelectionDescriptor_Struct Struct | For a rectangle deselection, the fields ** Deselection **, ** MultipleSelection **, ** Rectangle ** bits would be set. |
Method Detail¶
AddToSelectionList¶
-
Selection.
AddToSelectionList
¶ Add objects to the selection list.
Any objects already in the selection list are ignored. Use this function with UIStyler dialogs. You can call this from the constructor callback/selection initialization procedure to begin the dialog with objects already selected. The user can then review these objects, and if desired, deselect them.
The application selection callback can also call this function to add other objects to the selection list based on the objects(s) just selected. The selection filter procedure cannot call this function. Based on the object(s) just selected, other objects may need to be selected. For example, all edges of the selected face or all faces tangent to the selected face.
Signature
AddToSelectionList(select, objs, highlightFlag)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - objs (list of
NXOpen.NXObject
) – Objects to be added in the selection list - highlightFlag (bool) – If true, highlight objects
New in version NX5.0.0.
Deprecated since version NX8.0.0: Use
Selection.AddToTaggedObjectsSelectionList
insteadLicense requirements: None.
- select (
AddToTaggedObjectsSelectionList¶
-
Selection.
AddToTaggedObjectsSelectionList
¶ Add objects to the selection list.
Any objects already in the selection list are ignored. Use this function with UIStyler dialogs. You can call this from the constructor callback/selection initialization procedure to begin the dialog with objects already selected. The user can then review these objects, and if desired, deselect them.
The application selection callback can also call this function to add other objects to the selection list based on the objects(s) just selected. The selection filter procedure cannot call this function. Based on the object(s) just selected, other objects may need to be selected. For example, all edges of the selected face or all faces tangent to the selected face.
Signature
AddToTaggedObjectsSelectionList(select, objs, highlightFlag)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - objs (list of
NXOpen.TaggedObject
) – Objects to be added in the selection list - highlightFlag (bool) – If true, highlight objects
New in version NX7.5.4.
License requirements: None.
- select (
AskSelectionCursorPosition¶
-
Selection.
AskSelectionCursorPosition
¶ Returns the view and absolute coordinates of the cursor position for the associated selection.
If an object was selected, the view returned is the view in which the object was selected. For single position, the view is the view of the cursor. If the object was selected by name, view = None and the cursor position is undefined.
Signature
AskSelectionCursorPosition(select)
Parameters: select ( NXOpen.SelectionHandle
) – Selection handleReturns: a tuple Return type: A tuple consisting of (position, view). position is a NXOpen.Point3d
. view is aNXOpen.View
.New in version NX5.0.0.
License requirements: None.
AskSelectionDescriptor¶
-
Selection.
AskSelectionDescriptor
¶ Returns the information in
SelectionSelectionDescriptor_Struct
describing the selection that was just performed.Signature
AskSelectionDescriptor(select)
Parameters: select ( NXOpen.SelectionHandle
) –Returns: Return type: NXOpen.SelectionSelectionDescriptor_Struct
New in version NX5.0.0.
License requirements: None.
AskSelectionListCount¶
-
Selection.
AskSelectionListCount
¶ Returns the number of objects currently selected.
Use this function with UIStyler dialogs.
Signature
AskSelectionListCount(select)
Parameters: select ( NXOpen.SelectionHandle
) – Selection handleReturns: Count of objects selected Return type: int New in version NX5.0.0.
License requirements: None.
AskSelectionObjectList¶
-
Selection.
AskSelectionObjectList
¶ Returns the number of objects selected and a pointer to an array of tags of the objects selected.
Use this function with UIStyler dialogs.
Signature
AskSelectionObjectList(select)
Parameters: select ( NXOpen.SelectionHandle
) – Selection handleReturns: Selected objects. Return type: list of NXOpen.NXObject
New in version NX5.0.0.
Deprecated since version NX8.0.0: Use
Selection.AskSelectionTaggedObjectList
insteadLicense requirements: None.
AskSelectionRectanglePosition¶
-
Selection.
AskSelectionRectanglePosition
¶ Returns the absolute coordinates of the rectangle cursor positions.
The view that returns is the view of the button down position.
button down position - is the position where you press and hold mouse button 1. button up position - is the position where you release mouse button 1.
Pos1 and Pos2 are the absolute coordinates of the button down and button up positions respectively. Pos3 is the absolute coordinates of the rectangle corner which, as viewed on the screen, is horizontal with pos1. Pos4 is the absolute coordinates of the rectangle corner which, as viewed on the screen, is horizontal with pos2. Returns an error if the last gesture was not rectangle.
Signature
AskSelectionRectanglePosition(select)
Parameters: select ( NXOpen.SelectionHandle
) – Selection handleReturns: a tuple Return type: A tuple consisting of (view, position1, position2, position3, position4). view is a NXOpen.View
. View of button down position position1 is aNXOpen.Point3d
. Absolute coordinates of the button down position position2 is aNXOpen.Point3d
. Absolute coordinates of the button up position position3 is aNXOpen.Point3d
. Absolute coordinates of corner of screen rectangle which is horizontal with button down positionposition4 is aNXOpen.Point3d
. Absolute coordinates of corner of screen rectangle which is horizontal with button up positionNew in version NX5.0.0.
License requirements: None.
AskSelectionTaggedObjectList¶
-
Selection.
AskSelectionTaggedObjectList
¶ Returns the number of tagged objects selected and a pointer to an array of tags of the objects selected.
Use this function with UIStyler dialogs.
Signature
AskSelectionTaggedObjectList(select)
Parameters: select ( NXOpen.SelectionHandle
) – Selection handleReturns: Selected objects. Return type: list of NXOpen.TaggedObject
New in version NX7.5.4.
License requirements: None.
GetNumSelectedObjects¶
-
Selection.
GetNumSelectedObjects
¶ Returns the number of objects currently selected
Signature
GetNumSelectedObjects()
Returns: The number of objects currently selected Return type: int New in version NX3.0.0.
License requirements: None.
GetSelectedObject¶
-
Selection.
GetSelectedObject
¶ Returns the n’th object on the selection list
Signature
GetSelectedObject(index)
Parameters: index (int) – The index. Should be between 0 and GetNumSelectedObjects
Returns: The object at the given position on the selection list. Returns None if the index parameter is greater than the length of the list :rtype:
NXOpen.NXObject
New in version NX3.0.0.
Deprecated since version NX8.0.0: Use
Selection.GetSelectedTaggedObject
insteadLicense requirements: None.
GetSelectedTaggedObject¶
-
Selection.
GetSelectedTaggedObject
¶ Returns the n’th tagged object on the selection list
Signature
GetSelectedTaggedObject(index)
Parameters: index (int) – The index. Should be between 0 and GetNumSelectedObjects
Returns: The object at the given position on the selection list. Returns None if the index parameter is greater than the length of the list :rtype:
NXOpen.TaggedObject
New in version NX7.5.4.
License requirements: None.
GetSelectionStatusOfUserDefinedClass¶
-
Selection.
GetSelectionStatusOfUserDefinedClass
¶ Gets whether or not the user defined class is available for selection.
Signature
GetSelectionStatusOfUserDefinedClass(udoClass)
Parameters: udoClass ( NXOpen.UserDefinedObjects.UserDefinedClass
) – The UserDefinedClass in questionReturns: Allow the selection of this UserDefinedClass Return type: bool New in version NX5.0.0.
License requirements: None.
IsObjectInSelectionList¶
-
Selection.
IsObjectInSelectionList
¶ Inquires if object is selected.
Use this function with UIStyler dialogs.
Signature
IsObjectInSelectionList(select, object)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - object (
NXOpen.TaggedObject
) – Object
Returns: If true, object is in the selection list, else false.
Return type: bool
New in version NX5.0.0.
License requirements: None.
- select (
RemoveAllFromSelectionList¶
-
Selection.
RemoveAllFromSelectionList
¶ Removes all the objects from the selection list and optionally unhighlights them.
Use this function with UIStyler dialogs.
Signature
RemoveAllFromSelectionList(select, unhighlight)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - unhighlight (bool) – If true, unhighlight objects
New in version NX5.0.0.
License requirements: None.
- select (
RemoveFromSelectionList¶
-
Selection.
RemoveFromSelectionList
¶ Removes objects from the selection list.
Use this function with UIStyler dialogs. It can be called from the selection callback. It cannot be called from the selection filter procedure.
If any of the objects are not in the list, an error is returned and NO objects are removed from the list.
It could be called by the selection callback to remove objects from the selection list. For example, based on objects just deselected, the application may need to remove other associated objects from the selection list.
Signature
RemoveFromSelectionList(select, objs, unhighlight)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - objs (list of
NXOpen.NXObject
) – Array of object - unhighlight (bool) – If true, unhighlight objects
New in version NX5.0.0.
Deprecated since version NX8.0.0: Use
Selection.RemoveTaggedObjectsFromSelectionList
insteadLicense requirements: None.
- select (
RemoveTaggedObjectsFromSelectionList¶
-
Selection.
RemoveTaggedObjectsFromSelectionList
¶ Removes tagged objects from the selection list.
Use this function with UIStyler dialogs. It can be called from the selection callback. It cannot be called from the selection filter procedure.
If any of the objects are not in the list, an error is returned and NO objects are removed from the list.
It could be called by the selection callback to remove objects from the selection list. For example, based on objects just deselected, the application may need to remove other associated objects from the selection list.
Signature
RemoveTaggedObjectsFromSelectionList(select, objs, unhighlight)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - objs (list of
NXOpen.TaggedObject
) – Array of object - unhighlight (bool) – If true, unhighlight objects
New in version NX7.5.4.
License requirements: None.
- select (
SelectFeatures¶
-
Selection.
SelectFeatures
¶ Select features
Signature
SelectFeatures(message, featType)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- featType (
NXOpen.SelectionSelectionFeatureType
) – The types of features that are selectable
Returns: a tuple
Return type: A tuple consisting of (response, featureArray). response is a
NXOpen.SelectionResponse
. Ok, Back, or Cancel featureArray is a list ofNXOpen.Features.Feature
. The selected featuresNew in version NX3.0.0.
License requirements: None.
SelectObject¶
-
Selection.
SelectObject
¶ Overloaded method SelectObject
SelectObject(message, title, scope, includeFeatures, keepHighlighted)
SelectObject(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
SelectObject(message, title, scope, keepHighlighted, typeArray)
-------------------------------------
Select single object.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectObject(message, title, scope, includeFeatures, keepHighlighted)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
Returns: a tuple
Return type: A tuple consisting of (response, object, cursor). response is a
NXOpen.SelectionResponse
. Ok, Back, Cancel, ObjectSelected, or ObjectSelectedByName object is aNXOpen.NXObject
. The selected object cursor is aNXOpen.Point3d
. Absolute coordinates of cursor position. This is undefined if object is selected by nameNew in version NX3.0.0.
Deprecated since version NX8.0.0: Use
Selection.SelectTaggedObject
insteadLicense requirements: None.
-------------------------------------
Select single object using filter defined by mask triples. To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectObject(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - action (
NXOpen.SelectionSelectionAction
) – Indicates how the mask array will modify the selection filter - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- maskArray (list of
NXOpen.SelectionMaskTriple_Struct
) – Modifies the list of object types that can be selected. How it modifies the list of object types is determined by the SelectionAction parameter.
Returns: a tuple
Return type: A tuple consisting of (response, object, cursor). response is a
NXOpen.SelectionResponse
. Ok, Back, Cancel, ObjectSelected, or ObjectSelectedByName object is aNXOpen.NXObject
. The selected object cursor is aNXOpen.Point3d
. Absolute coordinates of cursor position. This is undefined if object is selected by nameNew in version NX3.0.0.
Deprecated since version NX8.0.0: Use
Selection.SelectTaggedObject
insteadLicense requirements: None.
-------------------------------------
Select single object using filter defined by selection type.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectObject(message, title, scope, keepHighlighted, typeArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- typeArray (list of
NXOpen.SelectionSelectionType
) – The types of objects that can be selected
Returns: a tuple
Return type: A tuple consisting of (response, object, cursor). response is a
NXOpen.SelectionResponse
. Ok, Back, Cancel, ObjectSelected, or ObjectSelectedByName object is aNXOpen.NXObject
. The selected object cursor is aNXOpen.Point3d
. Absolute coordinates of cursor position. This is undefined if object is selected by nameNew in version NX3.0.0.
Deprecated since version NX8.0.0: Use
Selection.SelectTaggedObject
insteadLicense requirements: None.
-------------------------------------
SelectObjects¶
-
Selection.
SelectObjects
¶ Overloaded method SelectObjects
SelectObjects(message, title, scope, includeFeatures, keepHighlighted)
SelectObjects(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
SelectObjects(message, title, scope, keepHighlighted, typeArray)
-------------------------------------
Select objects.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectObjects(message, title, scope, includeFeatures, keepHighlighted)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
Returns: a tuple
Return type: A tuple consisting of (response, objectArray). response is a
NXOpen.SelectionResponse
. Ok, Back, or Cancel objectArray is a list ofNXOpen.NXObject
. The selected objectsNew in version NX3.0.0.
Deprecated since version NX8.0.0: Use
Selection.SelectTaggedObjects
insteadLicense requirements: None.
-------------------------------------
Select objects using filter defined by mask triples.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectObjects(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - action (
NXOpen.SelectionSelectionAction
) – Indicates how the mask array will modify the selection filter - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- maskArray (list of
NXOpen.SelectionMaskTriple_Struct
) – Modifies the list of object types that can be selected. How it modifies the list of object types is determined by the SelectionAction parameter.
Returns: a tuple
Return type: A tuple consisting of (response, objectArray). response is a
NXOpen.SelectionResponse
. Ok, Back, or Cancel objectArray is a list ofNXOpen.NXObject
. The selected objectsNew in version NX3.0.0.
Deprecated since version NX8.0.0: Use
Selection.SelectTaggedObject
insteadLicense requirements: None.
-------------------------------------
Select objects using filter defined by selection type.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectObjects(message, title, scope, keepHighlighted, typeArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- typeArray (list of
NXOpen.SelectionSelectionType
) – The types that can be selected
Returns: a tuple
Return type: A tuple consisting of (response, objectArray). response is a
NXOpen.SelectionResponse
. Ok, Back, or Cancel objectArray is a list ofNXOpen.NXObject
. The selected objectsNew in version NX3.0.0.
Deprecated since version NX8.0.0: Use
Selection.SelectTaggedObject
insteadLicense requirements: None.
-------------------------------------
SelectScreenPosition¶
-
Selection.
SelectScreenPosition
¶ Select screen position on graphics display
Signature
SelectScreenPosition(message)
Parameters: message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter. Returns: a tuple Return type: A tuple consisting of (response, object, screenPosition). response is a NXOpen.SelectionDialogResponse
. Pick, Back, or Cancel object is aNXOpen.View
. View of selected screen location screenPosition is aNXOpen.Point3d
. Selected screen positionNew in version NX3.0.0.
License requirements: None.
SelectTaggedObject¶
-
Selection.
SelectTaggedObject
¶ Overloaded method SelectTaggedObject
SelectTaggedObject(message, title, scope, includeFeatures, keepHighlighted)
SelectTaggedObject(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
SelectTaggedObject(message, title, scope, keepHighlighted, typeArray)
-------------------------------------
Select single tagged object.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectTaggedObject(message, title, scope, includeFeatures, keepHighlighted)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
Returns: a tuple
Return type: A tuple consisting of (response, object, cursor). response is a
NXOpen.SelectionResponse
. Ok, Back, Cancel, ObjectSelected, or ObjectSelectedByName object is aNXOpen.TaggedObject
. The selected object cursor is aNXOpen.Point3d
. Absolute coordinates of cursor position. This is undefined if object is selected by nameNew in version NX7.5.4.
License requirements: None.
-------------------------------------
Select single tagged object using filter defined by mask triples. To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectTaggedObject(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - action (
NXOpen.SelectionSelectionAction
) – Indicates how the mask array will modify the selection filter - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- maskArray (list of
NXOpen.SelectionMaskTriple_Struct
) – Modifies the list of object types that can be selected. How it modifies the list of object types is determined by the SelectionAction parameter.
Returns: a tuple
Return type: A tuple consisting of (response, object, cursor). response is a
NXOpen.SelectionResponse
. Ok, Back, Cancel, ObjectSelected, or ObjectSelectedByName object is aNXOpen.TaggedObject
. The selected object cursor is aNXOpen.Point3d
. Absolute coordinates of cursor position. This is undefined if object is selected by nameNew in version NX7.5.4.
License requirements: None.
-------------------------------------
Select single tagged object using filter defined by selection type.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectTaggedObject(message, title, scope, keepHighlighted, typeArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- typeArray (list of
NXOpen.SelectionSelectionType
) – The types of objects that can be selected
Returns: a tuple
Return type: A tuple consisting of (response, object, cursor). response is a
NXOpen.SelectionResponse
. Ok, Back, Cancel, ObjectSelected, or ObjectSelectedByName object is aNXOpen.TaggedObject
. The selected object cursor is aNXOpen.Point3d
. Absolute coordinates of cursor position. This is undefined if object is selected by nameNew in version NX7.5.4.
License requirements: None.
-------------------------------------
SelectTaggedObjects¶
-
Selection.
SelectTaggedObjects
¶ Overloaded method SelectTaggedObjects
SelectTaggedObjects(message, title, scope, includeFeatures, keepHighlighted)
SelectTaggedObjects(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
SelectTaggedObjects(message, title, scope, keepHighlighted, typeArray)
-------------------------------------
Select tagged objects.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectTaggedObjects(message, title, scope, includeFeatures, keepHighlighted)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
Returns: a tuple
Return type: A tuple consisting of (response, objectArray). response is a
NXOpen.SelectionResponse
. Ok, Back, or Cancel objectArray is a list ofNXOpen.TaggedObject
. The selected objectsNew in version NX7.5.4.
License requirements: None.
-------------------------------------
Select tagged objects using filter defined by mask triples.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectTaggedObjects(message, title, scope, action, includeFeatures, keepHighlighted, maskArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - action (
NXOpen.SelectionSelectionAction
) – Indicates how the mask array will modify the selection filter - includeFeatures (bool) – Whether to allow the selection of features
- keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- maskArray (list of
NXOpen.SelectionMaskTriple_Struct
) – Modifies the list of object types that can be selected. How it modifies the list of object types is determined by the SelectionAction parameter.
Returns: a tuple
Return type: A tuple consisting of (response, objectArray). response is a
NXOpen.SelectionResponse
. Ok, Back, or Cancel objectArray is a list ofNXOpen.TaggedObject
. The selected objectsNew in version NX7.5.4.
License requirements: None.
-------------------------------------
Select tagged objects using filter defined by selection type.
To enable selection of objects within drawing member views, use SetCursorView API available on UFUi.
Signature
SelectTaggedObjects(message, title, scope, keepHighlighted, typeArray)
Parameters: - message (str) – Cue line message to display NOTE: The full Unicode character set is not supported for this parameter.
- title (str) – Dialog title NOTE: The full Unicode character set is not supported for this parameter.
- scope (
NXOpen.SelectionSelectionScope
) – Selection scope - keepHighlighted (bool) – Whether to keep the selection highlighted after it has been selected
- typeArray (list of
NXOpen.SelectionSelectionType
) – The types that can be selected
Returns: a tuple
Return type: A tuple consisting of (response, objectArray). response is a
NXOpen.SelectionResponse
. Ok, Back, or Cancel objectArray is a list ofNXOpen.TaggedObject
. The selected objectsNew in version NX7.5.4.
License requirements: None.
-------------------------------------
SetSelectType¶
-
Selection.
SetSelectType
¶ Sets the selection type.
It can be called from a callback to change the type of selection associated with the dialog.
Signature
SetSelectType(select, type)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - type (
NXOpen.SelectionUistylerSelectionType
) – Selection type
New in version NX5.0.0.
License requirements: None.
- select (
SetSelectionCallbacks¶
-
Selection.
SetSelectionCallbacks
¶ Specify selection filter callback for additional filtering based on application specific criteria, and/or selection callback to perform application specific processing for each selection gesture processed.
Both the filter callback and the selection callback are passed object to
SelectionHandle
which can be used to inquire other selection data or modify selection. This selection handle object is no longer valid after the filter callback or selection callback is exited.Signature
SetSelectionCallbacks(select, filterproc, selcb)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - filterproc (CallableObject) – Filter callback for additional user specificfiltering.
- selcb (CallableObject) – Selection callback for application specificprocessing.
New in version NX5.0.0.
Deprecated since version NX8.0.0: Use
Selection.SetTaggedObjectSelectionCallbacks
insteadLicense requirements: None.
- select (
SetSelectionMask¶
-
Selection.
SetSelectionMask
¶ Sets the types of objects that are selectable.
If this function is not called to set the mask, then the default mask is all standard types.
Signature
SetSelectionMask(select, action, maskArray)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - action (
NXOpen.SelectionSelectionAction
) – Mask action - maskArray (list of
NXOpen.SelectionMaskTriple_Struct
) – Mask triples
New in version NX5.0.0.
License requirements: None.
- select (
SetSelectionStatusOfUserDefinedClass¶
-
Selection.
SetSelectionStatusOfUserDefinedClass
¶ Sets whether or not the user defined class is available for selection.
Signature
SetSelectionStatusOfUserDefinedClass(udoClass, selectionStatus)
Parameters: - udoClass (
NXOpen.UserDefinedObjects.UserDefinedClass
) – The UserDefinedClass in question - selectionStatus (bool) – Allow the selection of this UserDefinedClass
New in version NX5.0.0.
License requirements: None.
- udoClass (
SetTaggedObjectSelectionCallbacks¶
-
Selection.
SetTaggedObjectSelectionCallbacks
¶ Specify selection filter callback for additional filtering of tagged objects based on application specific criteria, and/or selection callback to perform application specific processing for each selection gesture processed.
Both the filter callback and the selection callback are passed object to
SelectionHandle
which can be used to inquire other selection data or modify selection. This selection handle tagged object is no longer valid after the filter callback or selection callback is exited.Signature
SetTaggedObjectSelectionCallbacks(select, filterproc, selcb)
Parameters: - select (
NXOpen.SelectionHandle
) – Selection handle - filterproc (CallableObject) – Filter callback for additional user specificfiltering.
- selcb (CallableObject) – Selection callback for application specificprocessing.
New in version NX7.5.4.
License requirements: None.
- select (