SelectionSelectionDescriptor_Struct Struct¶
NXOpen.Selection.SelectionDescriptor is an alias for NXOpen.SelectionSelectionDescriptor_Struct
-
class
NXOpen.
SelectionSelectionDescriptor_Struct
¶ Bases:
object
For a rectangle deselection, the fields ** Deselection **, ** MultipleSelection **, ** Rectangle ** bits would be set.
For a name selection which selected one object, the fields ** SelectionDescriptor.Selection **, ** SingleSelection **, and ** NameSelection ** bits would be set. If a reselect was done (an object is selected and the previous object selected is deselected), only the field ** SelectionDescriptor.Reselection ** bit is set. The fields ** SingleSelection ** and ** MultipleSelection ** bits are not set for position. The field ** Rectangle ** bit is set for rectangle selection, rectangle deselection, and rectangle position. This function can be used with UIStyler dialogs and can be called from either the selection filter procedure or the selection callback.
Fields¶
Field | Description |
---|---|
Selection | |
Deselection | |
Reselection | |
SingleSelection | |
MultipleSelection | |
SinglePosition | |
RectanglePosition | |
NameSelection | |
Rectangle |
Selection¶
-
SelectionSelectionDescriptor_Struct.
Selection
¶ -------------------------------------
Getter Method Signature
Selection()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
Selection(value)
Parameters: value (bool) –
Deselection¶
-
SelectionSelectionDescriptor_Struct.
Deselection
¶ -------------------------------------
Getter Method Signature
Deselection()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
Deselection(value)
Parameters: value (bool) –
Reselection¶
-
SelectionSelectionDescriptor_Struct.
Reselection
¶ -------------------------------------
Getter Method Signature
Reselection()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
Reselection(value)
Parameters: value (bool) –
SingleSelection¶
-
SelectionSelectionDescriptor_Struct.
SingleSelection
¶ -------------------------------------
Getter Method Signature
SingleSelection()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
SingleSelection(value)
Parameters: value (bool) –
MultipleSelection¶
-
SelectionSelectionDescriptor_Struct.
MultipleSelection
¶ -------------------------------------
Getter Method Signature
MultipleSelection()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
MultipleSelection(value)
Parameters: value (bool) –
SinglePosition¶
-
SelectionSelectionDescriptor_Struct.
SinglePosition
¶ -------------------------------------
Getter Method Signature
SinglePosition()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
SinglePosition(value)
Parameters: value (bool) –
RectanglePosition¶
-
SelectionSelectionDescriptor_Struct.
RectanglePosition
¶ -------------------------------------
Getter Method Signature
RectanglePosition()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
RectanglePosition(value)
Parameters: value (bool) –