SelectionSelectionAction Enumeration¶
NXOpen.Selection.SelectionAction is an alias for NXOpen.SelectionSelectionAction
-
class
NXOpen.
SelectionSelectionAction
¶ Bases:
object
Indicates the type of action to perform when an object is selected.
Enum Members
Enum Member Enum Member Description EnableAll Include objects in selectionEnableSpecific Include selected objects in selectionDisableSpecific Remove selected objects from selectionClearAndEnableSpecific Clear selection and include selected objectsAllAndDisableSpecific Select all objects except for selected objects-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-