SelectionDialogResponse Enumeration¶
NXOpen.Selection.DialogResponse is an alias for NXOpen.SelectionDialogResponse
-
class
NXOpen.
SelectionDialogResponse
¶ Bases:
object
Specify the user response for general dialogs.
Enum Members
Enum Member Enum Member Description None No ResponsePick User picked object on screenOk User selected OkCancel User selected CancelBack User selected Back (if applicable)Apply User selected ApplyHelp User selected Help-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-