PropertiesManager Class¶
-
class
NXOpen.
PropertiesManager
¶ Bases:
object
The PropertiesManager class provides methods to create Gateway Properties Builder objects.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateAssembliesGeneralPropertiesBuilder | Create the Assemblies. |
CreateAssembliesParameterPropertiesBuilder | Create the Assemblies. |
CreateAttributePropertiesBuilder | Create the AttributePropertiesBuilder @return |
CreateAttributeTemplatesBuilder | Create the AttributeTemplatesBuilder @return |
CreateCamGeneralPropertiesBuilder | Create the Cam. |
CreateFeatureGeneralPropertiesBuilder | Create the FeatureGeneralPropertiesBuilder @return |
CreateGeneralCAMPropertiesBuilder | Create the CAM. |
CreateMassPropertiesBuilder | Create the MassPropertiesBuilder @return |
CreateObjectGeneralPropertiesBuilder | Create the ObjectGeneralPropertiesBuilder @return |
CreatePreviewPropertiesBuilder | Create the PreviewPropertiesBuilder @return |
Method Detail¶
CreateAssembliesGeneralPropertiesBuilder¶
-
PropertiesManager.
CreateAssembliesGeneralPropertiesBuilder
¶ Create the Assemblies.
AssembliesGeneralPropertiesBuilder
Signature
CreateAssembliesGeneralPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder
New in version NX8.0.0.
License requirements: None.
CreateAssembliesParameterPropertiesBuilder¶
-
PropertiesManager.
CreateAssembliesParameterPropertiesBuilder
¶ Create the Assemblies.
AssembliesParameterPropertiesBuilder
Signature
CreateAssembliesParameterPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.Assemblies.AssembliesParameterPropertiesBuilder
New in version NX8.0.0.
License requirements: None.
CreateAttributePropertiesBuilder¶
-
PropertiesManager.
CreateAttributePropertiesBuilder
¶ Create the AttributePropertiesBuilder
Signature
CreateAttributePropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.AttributePropertiesBuilder
New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.AttributeManagerCreateAttributePropertiesBuilder_Struct
instead.License requirements: None.
CreateAttributeTemplatesBuilder¶
-
PropertiesManager.
CreateAttributeTemplatesBuilder
¶ Create the AttributeTemplatesBuilder
Signature
CreateAttributeTemplatesBuilder()
Returns: Return type: NXOpen.AttributeTemplatesBuilder
New in version NX8.0.0.
License requirements: None.
CreateCamGeneralPropertiesBuilder¶
-
PropertiesManager.
CreateCamGeneralPropertiesBuilder
¶ Create the Cam.
CamGeneralPropertiesBuilder
Signature
CreateCamGeneralPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.Cam.CamGeneralPropertiesBuilder
New in version NX8.0.0.
Deprecated since version NX9.0.1: Use
NXOpen.PropertiesManager.CreateGeneralCAMPropertiesBuilder
instead.License requirements: None.
CreateFeatureGeneralPropertiesBuilder¶
-
PropertiesManager.
CreateFeatureGeneralPropertiesBuilder
¶ Create the FeatureGeneralPropertiesBuilder
Signature
CreateFeatureGeneralPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.FeatureGeneralPropertiesBuilder
New in version NX8.0.0.
License requirements: None.
CreateGeneralCAMPropertiesBuilder¶
-
PropertiesManager.
CreateGeneralCAMPropertiesBuilder
¶ Create the CAM.
GeneralCAMPropertiesBuilder
Signature
CreateGeneralCAMPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.CAM.GeneralPropertiesBuilder
New in version NX9.0.1.
License requirements: None.
CreateMassPropertiesBuilder¶
-
PropertiesManager.
CreateMassPropertiesBuilder
¶ Create the MassPropertiesBuilder
Signature
CreateMassPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.MassPropertiesBuilder
New in version NX8.0.0.
License requirements: None.
CreateObjectGeneralPropertiesBuilder¶
-
PropertiesManager.
CreateObjectGeneralPropertiesBuilder
¶ Create the ObjectGeneralPropertiesBuilder
Signature
CreateObjectGeneralPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.ObjectGeneralPropertiesBuilder
New in version NX8.0.0.
License requirements: None.
CreatePreviewPropertiesBuilder¶
-
PropertiesManager.
CreatePreviewPropertiesBuilder
¶ Create the PreviewPropertiesBuilder
Signature
CreatePreviewPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.PreviewPropertiesBuilder
New in version NX8.0.0.
License requirements: None.