AssembliesParameterPropertiesBuilder Class¶
-
class
NXOpen.Assemblies.
AssembliesParameterPropertiesBuilder
¶ Bases:
NXOpen.Builder
Represents an
NXOpen.Assemblies.AssembliesParameterPropertiesBuilder
to be used for changing the name or modifying the positioning mixture status of a component.To create a new instance of this class, use
NXOpen.PropertiesManager.CreateAssembliesParameterPropertiesBuilder
Default values.
Property Value Arrangements IndividuallyPositioned New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Arrangements | Returns or sets the arrangements. |
SelectedObjects | Returns the selected object(s) list. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AssembliesParameterPropertiesBuilderArrangementOptions Enumeration | The positioning mixture status options |
Property Detail¶
Arrangements¶
-
AssembliesParameterPropertiesBuilder.
Arrangements
¶ Returns or sets the arrangements.
The positioning mixture status for the selected components. No action will take place if Mixed is set as the arrangement option.
-------------------------------------
Getter Method
Signature
Arrangements()
Returns: Return type: NXOpen.Assemblies.AssembliesParameterPropertiesBuilderArrangementOptions
New in version NX8.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
Arrangements(arrangements)
Parameters: arrangements ( NXOpen.Assemblies.AssembliesParameterPropertiesBuilderArrangementOptions
) –New in version NX8.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SelectedObjects¶
-
AssembliesParameterPropertiesBuilder.
SelectedObjects
¶ Returns the selected object(s) list.
This is the active list of components that will be modified by any parameter changes.
-------------------------------------
Getter Method
Signature
SelectedObjects()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
Validate¶
-
AssembliesParameterPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.