PreviewPropertiesBuilder Class¶
-
class
NXOpen.
PreviewPropertiesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.PreviewPropertiesBuilder
to be used for creating and storing previews.Both part previews and model view previews are supported.
To create a new instance of this class, use
NXOpen.PropertiesManager.CreatePreviewPropertiesBuilder
Default values.
Property Value ModelViewCreation OnPartSave PartCreation OnSave StoreModelViewPreview 0 StorePartPreview 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ModelViewCreation | Returns or sets the model view creation. |
PartCreation | Returns or sets the part creation. |
SelectedObjects | Returns the selected object(s) list. |
StoreModelViewPreview | Returns or sets the store model view preview. |
StorePartPreview | Returns or sets the store part preview. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreviewPropertiesBuilderModelViewCreationOptions Enumeration | Specifies when the model view preview will be created |
PreviewPropertiesBuilderPartCreationOptions Enumeration | Specifies when the part preview will be created |
Property Detail¶
ModelViewCreation¶
-
PreviewPropertiesBuilder.
ModelViewCreation
¶ Returns or sets the model view creation.
This option determines when the model view preview will be stored. It is only used if the store model view preview is turned on.
-------------------------------------
Getter Method
Signature
ModelViewCreation()
Returns: Return type: NXOpen.PreviewPropertiesBuilderModelViewCreationOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModelViewCreation(modelViewCreation)
Parameters: modelViewCreation ( NXOpen.PreviewPropertiesBuilderModelViewCreationOptions
) –New in version NX8.0.0.
License requirements: None.
PartCreation¶
-
PreviewPropertiesBuilder.
PartCreation
¶ Returns or sets the part creation.
This option determines when the part preview will be stored. It is only used if the store part preview is turned on.
-------------------------------------
Getter Method
Signature
PartCreation()
Returns: Return type: NXOpen.PreviewPropertiesBuilderPartCreationOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartCreation(partCreation)
Parameters: partCreation ( NXOpen.PreviewPropertiesBuilderPartCreationOptions
) –New in version NX8.0.0.
License requirements: None.
SelectedObjects¶
-
PreviewPropertiesBuilder.
SelectedObjects
¶ Returns the selected object(s) list.
-------------------------------------
Getter Method
Signature
SelectedObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
StoreModelViewPreview¶
-
PreviewPropertiesBuilder.
StoreModelViewPreview
¶ Returns or sets the store model view preview.
Determines if the model view preview will be stored. If true, the model view creation option will decide when the preview will be stored.
-------------------------------------
Getter Method
Signature
StoreModelViewPreview()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StoreModelViewPreview(storeModelViewPreview)
Parameters: storeModelViewPreview (bool) – New in version NX8.0.0.
License requirements: None.
StorePartPreview¶
-
PreviewPropertiesBuilder.
StorePartPreview
¶ Returns or sets the store part preview.
Determines if the part preview will be stored. If true, the part creation option will decide when the preview will be stored.
-------------------------------------
Getter Method
Signature
StorePartPreview()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StorePartPreview(storePartPreview)
Parameters: storePartPreview (bool) – New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PreviewPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.