AssembliesGeneralPropertiesBuilder Class¶
-
class
NXOpen.Assemblies.
AssembliesGeneralPropertiesBuilder
¶ Bases:
NXOpen.Builder
Represents an
NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder
to be used for changing the general properties of a component.To create a new instance of this class, use
NXOpen.PropertiesManager.CreateAssembliesGeneralPropertiesBuilder
Default values.
Property Value Hidden No IntegerQuantity 0 Layer 0 LayerOption OriginalLayer NonGeometric 0 QuantityType Number RealQuantity 0 ReferenceComponent No SpecificColor 0 SpecificPartialShade 0 SpecificTranslucency 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Hidden | Returns or sets the hidden option. |
IntegerQuantity | Returns or sets the integer quantity. |
Layer | Returns or sets the layer. |
LayerOption | Returns or sets the layer option. |
NonGeometric | Returns or sets the non geometric flag. |
QuantityType | Returns or sets the quantity type. |
RealQuantity | Returns or sets the real quantity. |
ReferenceComponent | Returns or sets the reference-only component flag. |
SelectedObjects | Returns the selected object(s) list. |
SpecificColor | Returns or sets the specific color flag. |
SpecificPartialShade | Returns or sets the specific partial shade flag. |
SpecificTranslucency | Returns or sets the specific translucency flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SynchronizeAttributes | Synchronize the attributes on the components |
SynchronizeDisplay | Synchronize the display on the components |
SynchronizeLayers | Synchronize the layers on the components |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AssembliesGeneralPropertiesBuilderHiddenOptions Enumeration | Options for managing the hidden property on the components |
AssembliesGeneralPropertiesBuilderLayerOptions Enumeration | Layer options for the components |
AssembliesGeneralPropertiesBuilderQuantityOptions Enumeration | Options for assigning the quantity on the components |
AssembliesGeneralPropertiesBuilderReferenceComponentOptions Enumeration | Options for setting the reference-only property on the components |
Property Detail¶
IntegerQuantity¶
-
AssembliesGeneralPropertiesBuilder.
IntegerQuantity
¶ Returns or sets the integer quantity.
This value will be used if the Quantity Type is set to Number and the DB_UNITS attribute is not set.
-------------------------------------
Getter Method
Signature
IntegerQuantity()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntegerQuantity(integerQuantity)
Parameters: integerQuantity (int) – New in version NX8.0.0.
License requirements: None.
Layer¶
-
AssembliesGeneralPropertiesBuilder.
Layer
¶ Returns or sets the layer.
Used if the layer option is set to specified.
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX8.0.0.
License requirements: None.
LayerOption¶
-
AssembliesGeneralPropertiesBuilder.
LayerOption
¶ Returns or sets the layer option.
If specified layer is set, then the layer will be used.
-------------------------------------
Getter Method
Signature
LayerOption()
Returns: Return type: NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderLayerOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayerOption(layerOption)
Parameters: layerOption ( NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderLayerOptions
) –New in version NX8.0.0.
License requirements: None.
NonGeometric¶
-
AssembliesGeneralPropertiesBuilder.
NonGeometric
¶ Returns or sets the non geometric flag.
Sets the components to either geometric or non-geometric.
-------------------------------------
Getter Method
Signature
NonGeometric()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonGeometric(nonGeometric)
Parameters: nonGeometric (bool) – New in version NX8.0.0.
License requirements: None.
QuantityType¶
-
AssembliesGeneralPropertiesBuilder.
QuantityType
¶ Returns or sets the quantity type.
If the quantity type is set to number than either the integer quantity or the real quantity values will be used. Otherwise the quantity will be set to as-required.
-------------------------------------
Getter Method
Signature
QuantityType()
Returns: Return type: NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderQuantityOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QuantityType(quantityType)
Parameters: quantityType ( NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderQuantityOptions
) –New in version NX8.0.0.
License requirements: None.
RealQuantity¶
-
AssembliesGeneralPropertiesBuilder.
RealQuantity
¶ Returns or sets the real quantity.
This value will be used if the Quantity Type is set to Number and the DB_UNITS attribute has been set.
-------------------------------------
Getter Method
Signature
RealQuantity()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RealQuantity(realQuantity)
Parameters: realQuantity (float) – New in version NX8.0.0.
License requirements: None.
ReferenceComponent¶
-
AssembliesGeneralPropertiesBuilder.
ReferenceComponent
¶ Returns or sets the reference-only component flag.
This option determines whether the components will be reference-only or not.
-------------------------------------
Getter Method
Signature
ReferenceComponent()
Returns: Return type: NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderReferenceComponentOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceComponent(referenceComponent)
Parameters: referenceComponent ( NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderReferenceComponentOptions
) –New in version NX8.0.0.
License requirements: None.
SelectedObjects¶
-
AssembliesGeneralPropertiesBuilder.
SelectedObjects
¶ Returns the selected object(s) list.
This is the active list of components that will be modified by any changes.
-------------------------------------
Getter Method
Signature
SelectedObjects()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
SpecificColor¶
-
AssembliesGeneralPropertiesBuilder.
SpecificColor
¶ Returns or sets the specific color flag.
The explicit color display property will be discarded from all components.
-------------------------------------
Getter Method
Signature
SpecificColor()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecificColor(specificColor)
Parameters: specificColor (bool) – New in version NX8.0.0.
License requirements: None.
SpecificPartialShade¶
-
AssembliesGeneralPropertiesBuilder.
SpecificPartialShade
¶ Returns or sets the specific partial shade flag.
The explicit partial shade display property will be discarded from all components.
-------------------------------------
Getter Method
Signature
SpecificPartialShade()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecificPartialShade(specificPartialShade)
Parameters: specificPartialShade (bool) – New in version NX8.0.0.
License requirements: None.
SpecificTranslucency¶
-
AssembliesGeneralPropertiesBuilder.
SpecificTranslucency
¶ Returns or sets the specific translucency flag.
The explicit translucency display property will be discarded from all components.
-------------------------------------
Getter Method
Signature
SpecificTranslucency()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecificTranslucency(specificTranslucency)
Parameters: specificTranslucency (bool) – New in version NX8.0.0.
License requirements: None.
Method Detail¶
SynchronizeAttributes¶
-
AssembliesGeneralPropertiesBuilder.
SynchronizeAttributes
¶ Synchronize the attributes on the components
Signature
SynchronizeAttributes()
New in version NX8.0.0.
License requirements: None.
SynchronizeDisplay¶
-
AssembliesGeneralPropertiesBuilder.
SynchronizeDisplay
¶ Synchronize the display on the components
Signature
SynchronizeDisplay()
New in version NX8.0.0.
License requirements: None.
SynchronizeLayers¶
-
AssembliesGeneralPropertiesBuilder.
SynchronizeLayers
¶ Synchronize the layers on the components
Signature
SynchronizeLayers()
New in version NX8.0.0.
License requirements: None.
Validate¶
-
AssembliesGeneralPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.