ObjectGeneralPropertiesBuilder Class¶
-
class
NXOpen.
ObjectGeneralPropertiesBuilder
¶ Bases:
NXOpen.Builder
Represents an
NXOpen.ObjectGeneralPropertiesBuilder
to be used for modifying the names and properties of objects.To create a new instance of this class, use
NXOpen.PropertiesManager.CreateObjectGeneralPropertiesBuilder
Default values.
Property Value Active 0 AddComponents 0 AddIndex 0 ApplyToComponent 0 Index 0 TopLevel 0 UniqueMembership 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Active | Returns or sets the active. |
AddComponents | Returns or sets the add components. |
AddIndex | Returns or sets the add index. |
ApplyToComponent | Returns or sets the apply to component. |
GroupDisplayProperties | Returns or sets the group display properties. |
Index | Returns or sets the index. |
Name | Returns or sets the name. |
NameLocationSpecified | Returns or sets the name location specified. |
SelectedObjects | Returns the selected object(s) list. |
Tag | Returns the Tag for this object. |
TopLevel | Returns or sets the top level. |
UniqueMembership | Returns or sets the unique membership. |
Methods¶
Method | Description |
---|---|
ApplyToAllOccurrences | Apply name to the instance of the component. |
Commit | Commits any edits that have been applied to the builder. |
Delete | Delete the name of each selected object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNameLocation | Gets the name location @return |
GetObject | Returns the object currently being edited by this builder. |
SetNameLocation | Sets the name location. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Active¶
-
ObjectGeneralPropertiesBuilder.
Active
¶ Returns or sets the active.
This will activate or deactivate a group.
-------------------------------------
Getter Method
Signature
Active()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Active(active)
Parameters: active (bool) – New in version NX8.0.0.
License requirements: None.
AddComponents¶
-
ObjectGeneralPropertiesBuilder.
AddComponents
¶ Returns or sets the add components.
This flag determines whether new components will be added automatically.
-------------------------------------
Getter Method
Signature
AddComponents()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddComponents(addComponents)
Parameters: addComponents (bool) – New in version NX8.0.0.
License requirements: None.
AddIndex¶
-
ObjectGeneralPropertiesBuilder.
AddIndex
¶ Returns or sets the add index.
An index will be appended to the name if this is set to true.
-------------------------------------
Getter Method
Signature
AddIndex()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddIndex(addIndex)
Parameters: addIndex (bool) – New in version NX8.0.0.
License requirements: None.
ApplyToComponent¶
-
ObjectGeneralPropertiesBuilder.
ApplyToComponent
¶ Returns or sets the apply to component.
The name will be applied to the component if this is true.
-------------------------------------
Getter Method
Signature
ApplyToComponent()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyToComponent(applyToComponent)
Parameters: applyToComponent (bool) – New in version NX8.0.0.
License requirements: None.
GroupDisplayProperties¶
-
ObjectGeneralPropertiesBuilder.
GroupDisplayProperties
¶ Returns or sets the group display properties.
This field manages the display properties on a group.
-------------------------------------
Getter Method
Signature
GroupDisplayProperties()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GroupDisplayProperties(groupDisplayProperties)
Parameters: groupDisplayProperties (bool) – New in version NX8.0.0.
License requirements: None.
Index¶
-
ObjectGeneralPropertiesBuilder.
Index
¶ Returns or sets the index.
The index to be appended to the name if “Add Index” is set to true.
-------------------------------------
Getter Method
Signature
Index()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Index(index)
Parameters: index (int) – New in version NX8.0.0.
License requirements: None.
Name¶
-
ObjectGeneralPropertiesBuilder.
Name
¶ Returns or sets the name.
The new name that will be applied to the selected objects.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX8.0.0.
License requirements: None.
NameLocationSpecified¶
-
ObjectGeneralPropertiesBuilder.
NameLocationSpecified
¶ Returns or sets the name location specified.
This states whether the name location will be changed.
-------------------------------------
Getter Method
Signature
NameLocationSpecified()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NameLocationSpecified(nameLocationSpecified)
Parameters: nameLocationSpecified (bool) – New in version NX8.0.0.
License requirements: None.
SelectedObjects¶
-
ObjectGeneralPropertiesBuilder.
SelectedObjects
¶ Returns the selected object(s) list.
-------------------------------------
Getter Method
Signature
SelectedObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
TopLevel¶
-
ObjectGeneralPropertiesBuilder.
TopLevel
¶ Returns or sets the top level.
This object will be displayed at the top level of the part navigator if this is set to true. Only applies if the object selected is a group or a reference set.
-------------------------------------
Getter Method
Signature
TopLevel()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TopLevel(topLevel)
Parameters: topLevel (bool) – New in version NX8.0.0.
License requirements: None.
UniqueMembership¶
-
ObjectGeneralPropertiesBuilder.
UniqueMembership
¶ Returns or sets the unique membership.
This field manages the unique membership property on a group.
-------------------------------------
Getter Method
Signature
UniqueMembership()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UniqueMembership(uniqueMembership)
Parameters: uniqueMembership (bool) – New in version NX8.0.0.
License requirements: None.
Method Detail¶
ApplyToAllOccurrences¶
-
ObjectGeneralPropertiesBuilder.
ApplyToAllOccurrences
¶ Apply name to the instance of the component.
All occurrences of the instance will inherit this name.
Signature
ApplyToAllOccurrences()
New in version NX8.0.0.
License requirements: None.
Delete¶
-
ObjectGeneralPropertiesBuilder.
Delete
¶ Delete the name of each selected object.
Signature
Delete()
New in version NX8.0.0.
License requirements: None.
GetNameLocation¶
-
ObjectGeneralPropertiesBuilder.
GetNameLocation
¶ Gets the name location
Signature
GetNameLocation()
Returns: Return type: NXOpen.Point3d
New in version NX8.0.0.
License requirements: None.
SetNameLocation¶
-
ObjectGeneralPropertiesBuilder.
SetNameLocation
¶ Sets the name location.
If name location specified is true, this value will be used to change the name location of the general object.
Signature
SetNameLocation(nameLocation)
Parameters: nameLocation ( NXOpen.Point3d
) – the name locationNew in version NX8.0.0.
License requirements: None.
Validate¶
-
ObjectGeneralPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.