GanttCollection Class¶
-
class
NXOpen.Mechatronics.
GanttCollection
¶ Bases:
object
Represents a
NXOpen.Mechatronics.GanttCollection
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateGanttExportPlcopenBuilder | Creates a NXOpen.Mechatronics.GanttExportPLCopenBuilder @return |
CreateGanttOperationBuilder | Creates a NXOpen.Mechatronics.GanttOperationBuilder @return |
CreateGanttOperationConditionBuilder | Creates a NXOpen.Mechatronics.GanttOperationConditionBuilder @return |
CreateGanttOperationParameterBuilder | Creates a NXOpen.Mechatronics.GanttOperationParameterBuilder @return |
FindObject | Finds the NXOpen.Mechatronics.GanttOperationObject with the given name. |
Method Detail¶
CreateGanttExportPlcopenBuilder¶
-
GanttCollection.
CreateGanttExportPlcopenBuilder
¶ Creates a
NXOpen.Mechatronics.GanttExportPLCopenBuilder
Signature
CreateGanttExportPlcopenBuilder(object)
Parameters: object ( NXOpen.Mechatronics.GanttOperationObject
) –Returns: Return type: NXOpen.Mechatronics.GanttExportPLCopenBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateGanttOperationBuilder¶
-
GanttCollection.
CreateGanttOperationBuilder
¶ Creates a
NXOpen.Mechatronics.GanttOperationBuilder
Signature
CreateGanttOperationBuilder(object)
Parameters: object ( NXOpen.Mechatronics.GanttOperationObject
) –Returns: Return type: NXOpen.Mechatronics.GanttOperationBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateGanttOperationConditionBuilder¶
-
GanttCollection.
CreateGanttOperationConditionBuilder
¶ Creates a
NXOpen.Mechatronics.GanttOperationConditionBuilder
Signature
CreateGanttOperationConditionBuilder()
Returns: Return type: NXOpen.Mechatronics.GanttOperationConditionBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateGanttOperationParameterBuilder¶
-
GanttCollection.
CreateGanttOperationParameterBuilder
¶ Creates a
NXOpen.Mechatronics.GanttOperationParameterBuilder
Signature
CreateGanttOperationParameterBuilder()
Returns: Return type: NXOpen.Mechatronics.GanttOperationParameterBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
GanttCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.GanttOperationObject
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.GanttOperationObject
.Returns: NXOpen.Mechatronics.GanttOperationObject
with this name.Return type: NXOpen.Mechatronics.GanttOperationObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)