GanttOperationParameterBuilder Class¶
-
class
NXOpen.Mechatronics.
GanttOperationParameterBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.GanttOperationParameterBuilder
To create a new instance of this class, use
NXOpen.Mechatronics.GanttCollection.CreateGanttOperationParameterBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
ExpressionValue | Returns the expression value for double and interger parameters |
IOStatus | Returns or sets the io status |
ObjectValue | Returns or sets the parameter value which will be set to the input physics object during runtime. |
Operator | Returns or sets the operator value. |
ParameterName | Returns or sets the parameter name |
ParameterValue | Returns or sets the parameter value which will be set to the input physics object during runtime. |
PropertyId | Returns or sets the id of property in physics object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PutExpressionValue | Set the expression value for double and interger parameters |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GanttOperationParameterBuilderOperatorOption Enumeration | the Operator options. |
Property Detail¶
ExpressionValue¶
-
GanttOperationParameterBuilder.
ExpressionValue
¶ Returns the expression value for double and interger parameters
-------------------------------------
Getter Method
Signature
ExpressionValue()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
IOStatus¶
-
GanttOperationParameterBuilder.
IOStatus
¶ Returns or sets the io status
-------------------------------------
Getter Method
Signature
IOStatus()
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
IOStatus(io)
Parameters: io (bool) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ObjectValue¶
-
GanttOperationParameterBuilder.
ObjectValue
¶ Returns or sets the parameter value which will be set to the input physics object during runtime.
If property value type is not object, this property should be null, it can be a physics object(Rigid Body, Collision, Constraints, Joints etc.), Function Table, Material etc.
-------------------------------------
Getter Method
Signature
ObjectValue()
Returns: Return type: NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ObjectValue(objValue)
Parameters: objValue ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Operator¶
-
GanttOperationParameterBuilder.
Operator
¶ Returns or sets the operator value.
-------------------------------------
Getter Method
Signature
Operator()
Returns: Return type: NXOpen.Mechatronics.GanttOperationParameterBuilderOperatorOption
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Operator(optr)
Parameters: optr ( NXOpen.Mechatronics.GanttOperationParameterBuilderOperatorOption
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParameterName¶
-
GanttOperationParameterBuilder.
ParameterName
¶ Returns or sets the parameter name
-------------------------------------
Getter Method
Signature
ParameterName()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ParameterName(name)
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParameterValue¶
-
GanttOperationParameterBuilder.
ParameterValue
¶ Returns or sets the parameter value which will be set to the input physics object during runtime.
-------------------------------------
Getter Method
Signature
ParameterValue()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ParameterValue(strValue)
Parameters: strValue (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PropertyId¶
-
GanttOperationParameterBuilder.
PropertyId
¶ Returns or sets the id of property in physics object
-------------------------------------
Getter Method
Signature
PropertyId()
Returns: Return type: int New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PropertyId(prop)
Parameters: prop (int) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
PutExpressionValue¶
-
GanttOperationParameterBuilder.
PutExpressionValue
¶ Set the expression value for double and interger parameters
Signature
PutExpressionValue(exp)
Parameters: exp ( NXOpen.Expression
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
GanttOperationParameterBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.