GanttOperationParameterBuilderOperatorOption Enumeration¶
NXOpen.Mechatronics.GanttOperationParameterBuilder.OperatorOption is an alias for NXOpen.Mechatronics.GanttOperationParameterBuilderOperatorOption
-
class
NXOpen.Mechatronics.
GanttOperationParameterBuilderOperatorOption
¶ Bases:
object
the Operator options.
Enum Members
Enum Member Enum Member Description None Increment Increment operator ‘+=’Decrement Decrement operator ‘-=’Multiply Multiply operator ‘*=’Not Not operator-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-