GanttOperationConditionBuilder Class¶
-
class
NXOpen.Mechatronics.
GanttOperationConditionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.GanttOperationConditionBuilder
To create a new instance of this class, use
NXOpen.Mechatronics.GanttCollection.CreateGanttOperationConditionBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
Condition | Returns or sets the judging condition from current condition,the value can be ‘And’ or ‘Or’ |
ConditionId | Returns or sets the id of condition |
ConditionValue | Returns or sets the condition value use to evaluate this condition for the selected property in condition object |
ExpressionValue | Returns the expression value for double and interger parameters |
Index | Returns or sets the sequence number of condition |
IsGroup | Returns or sets the condition type, if the condition is a group, the value is ‘true’ |
ObjectValue | Returns or sets the condition value use to evaluate this condition for the selected property in condition object. |
OperatorValue | Returns or sets the operator of current condition |
ParentId | Returns or sets the parent id of condition |
PhysicsObject | Returns or sets the conditin object :it can be a physics object(Rigid Body, Collision, Constraints, Joints etc. |
PropertyId | Returns or sets the selected property id in physics object |
PropertyName | Returns or sets the name of selected property |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PutExpressionValue | Set the expression value for double and interger parameters |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Condition¶
-
GanttOperationConditionBuilder.
Condition
¶ Returns or sets the judging condition from current condition,the value can be ‘And’ or ‘Or’
-------------------------------------
Getter Method
Signature
Condition()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Condition(strCondition)
Parameters: strCondition (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ConditionId¶
-
GanttOperationConditionBuilder.
ConditionId
¶ Returns or sets the id of condition
-------------------------------------
Getter Method
Signature
ConditionId()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ConditionId(id)
Parameters: id (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ConditionValue¶
-
GanttOperationConditionBuilder.
ConditionValue
¶ Returns or sets the condition value use to evaluate this condition for the selected property in condition object
-------------------------------------
Getter Method
Signature
ConditionValue()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ConditionValue(strValue)
Parameters: strValue (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ExpressionValue¶
-
GanttOperationConditionBuilder.
ExpressionValue
¶ Returns the expression value for double and interger parameters
-------------------------------------
Getter Method
Signature
ExpressionValue()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Index¶
-
GanttOperationConditionBuilder.
Index
¶ Returns or sets the sequence number of condition
-------------------------------------
Getter Method
Signature
Index()
Returns: Return type: int New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Index(ind)
Parameters: ind (int) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
IsGroup¶
-
GanttOperationConditionBuilder.
IsGroup
¶ Returns or sets the condition type, if the condition is a group, the value is ‘true’
-------------------------------------
Getter Method
Signature
IsGroup()
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
IsGroup(isGroup)
Parameters: isGroup (bool) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ObjectValue¶
-
GanttOperationConditionBuilder.
ObjectValue
¶ Returns or sets the condition value use to evaluate this condition for the selected property in condition object.
If selected property value type is not object, this property should be null, it can be a physics object(Rigid Body, Collision, Constraints, Joints etc.), Function Table, Material etc.
-------------------------------------
Getter Method
Signature
ObjectValue()
Returns: Return type: NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ObjectValue(objValue)
Parameters: objValue ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
OperatorValue¶
-
GanttOperationConditionBuilder.
OperatorValue
¶ Returns or sets the operator of current condition
-------------------------------------
Getter Method
Signature
OperatorValue()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
OperatorValue(strOperator)
Parameters: strOperator (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParentId¶
-
GanttOperationConditionBuilder.
ParentId
¶ Returns or sets the parent id of condition
-------------------------------------
Getter Method
Signature
ParentId()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ParentId(parentId)
Parameters: parentId (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PhysicsObject¶
-
GanttOperationConditionBuilder.
PhysicsObject
¶ Returns or sets the conditin object :it can be a physics object(Rigid Body, Collision, Constraints, Joints etc.
), FunctionTable.
-------------------------------------
Getter Method
Signature
PhysicsObject()
Returns: Return type: NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PhysicsObject(physObj)
Parameters: physObj ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PropertyId¶
-
GanttOperationConditionBuilder.
PropertyId
¶ Returns or sets the selected property id in physics object
-------------------------------------
Getter Method
Signature
PropertyId()
Returns: Return type: int New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PropertyId(prop)
Parameters: prop (int) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PropertyName¶
-
GanttOperationConditionBuilder.
PropertyName
¶ Returns or sets the name of selected property
-------------------------------------
Getter Method
Signature
PropertyName()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PropertyName(name)
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
PutExpressionValue¶
-
GanttOperationConditionBuilder.
PutExpressionValue
¶ Set the expression value for double and interger parameters
Signature
PutExpressionValue(exp)
Parameters: exp ( NXOpen.Expression
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
GanttOperationConditionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.