GanttOperationBuilder Class¶
-
class
NXOpen.Mechatronics.
GanttOperationBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.GanttOperationBuilder
builderTo create a new instance of this class, use
NXOpen.Mechatronics.GanttCollection.CreateGanttOperationBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
ActiveStatus | Returns or sets the active status |
ConditionList | Returns the condition data |
Context | Returns or sets the owner part of operation |
Duration | Returns or sets the operation duration |
ExpressionDuration | Returns the operation duration expression |
OperationID | Returns or sets the operation id |
OperationName | Returns or sets the operation name |
OperationTypes | Returns or sets the operation type |
ParameterList | Returns the parameter data |
ParentID | Returns or sets the parent operation id in sequence editor tree |
Physics | Returns or sets the input of the operation : it can be a physics object(Rigid Body, Collision, Constraints, Joints etc. |
StartTime | Returns or sets the start time of operation |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of simple operation. |
Methods¶
Method | Description |
---|---|
AddConditionList | Sets the condition data |
AddParameterList | Sets the parameter data |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GanttOperationBuilderOperationType Enumeration | the operation Type enum |
GanttOperationBuilderSimpleOperationType Enumeration | the pause operation Type enum |
Property Detail¶
ActiveStatus¶
-
GanttOperationBuilder.
ActiveStatus
¶ Returns or sets the active status
-------------------------------------
Getter Method
Signature
ActiveStatus()
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ActiveStatus(status)
Parameters: status (bool) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ConditionList¶
-
GanttOperationBuilder.
ConditionList
¶ Returns the condition data
-------------------------------------
Getter Method
Signature
ConditionList()
Returns: Return type: NXOpen.Mechatronics.GanttOperationConditionBuilderList
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Context¶
-
GanttOperationBuilder.
Context
¶ Returns or sets the owner part of operation
-------------------------------------
Getter Method
Signature
Context()
Returns: Return type: NXOpen.BasePart
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Context(context)
Parameters: context ( NXOpen.BasePart
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Duration¶
-
GanttOperationBuilder.
Duration
¶ Returns or sets the operation duration
-------------------------------------
Getter Method
Signature
Duration()
Returns: Return type: float New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Duration(duration)
Parameters: duration (float) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ExpressionDuration¶
-
GanttOperationBuilder.
ExpressionDuration
¶ Returns the operation duration expression
-------------------------------------
Getter Method
Signature
ExpressionDuration()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
OperationID¶
-
GanttOperationBuilder.
OperationID
¶ Returns or sets the operation id
-------------------------------------
Getter Method
Signature
OperationID()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
OperationID(id)
Parameters: id (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
OperationName¶
-
GanttOperationBuilder.
OperationName
¶ Returns or sets the operation name
-------------------------------------
Getter Method
Signature
OperationName()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
OperationName(name)
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
OperationTypes¶
-
GanttOperationBuilder.
OperationTypes
¶ Returns or sets the operation type
-------------------------------------
Getter Method
Signature
OperationTypes()
Returns: Return type: NXOpen.Mechatronics.GanttOperationBuilderOperationType
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
OperationTypes(type)
Parameters: type ( NXOpen.Mechatronics.GanttOperationBuilderOperationType
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParameterList¶
-
GanttOperationBuilder.
ParameterList
¶ Returns the parameter data
-------------------------------------
Getter Method
Signature
ParameterList()
Returns: Return type: NXOpen.Mechatronics.GanttOperationParameterBuilderList
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParentID¶
-
GanttOperationBuilder.
ParentID
¶ Returns or sets the parent operation id in sequence editor tree
-------------------------------------
Getter Method
Signature
ParentID()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ParentID(parent)
Parameters: parent (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Physics¶
-
GanttOperationBuilder.
Physics
¶ Returns or sets the input of the operation : it can be a physics object(Rigid Body, Collision, Constraints, Joints etc.
), FunctionTable, part occurrence.
-------------------------------------
Getter Method
Signature
Physics()
Returns: Return type: NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Physics(physics)
Parameters: physics ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StartTime¶
-
GanttOperationBuilder.
StartTime
¶ Returns or sets the start time of operation
-------------------------------------
Getter Method
Signature
StartTime()
Returns: Return type: float New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
StartTime(start)
Parameters: start (float) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Type¶
-
GanttOperationBuilder.
Type
¶ Returns or sets the type of simple operation.
-------------------------------------
Getter Method
Signature
Type()
Returns: Indicates the current type value of the dialog’s types block Return type: NXOpen.Mechatronics.GanttOperationBuilderSimpleOperationType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Mechatronics.GanttOperationBuilderSimpleOperationType
) – Indicates the type value of the dialog’s types block to be set toNew in version NX9.0.0.
License requirements: None.
Method Detail¶
AddConditionList¶
-
GanttOperationBuilder.
AddConditionList
¶ Sets the condition data
Signature
AddConditionList(conditions)
Parameters: conditions (list of NXOpen.Mechatronics.GanttOperationConditionBuilder
) – Input conditionsNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AddParameterList¶
-
GanttOperationBuilder.
AddParameterList
¶ Sets the parameter data
Signature
AddParameterList(parameters)
Parameters: parameters (list of NXOpen.Mechatronics.GanttOperationParameterBuilder
) – Input parametersNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
GanttOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.