NXOpen.Facet Package¶
Classes¶
NXOpen.Facet.BestFitAlignBuilder |
This class performs the best fit alignment between objects |
NXOpen.Facet.BridgeFacetBodyBuilder |
Represents a NXOpen.Facet.BridgeFacetBodyBuilder It bridges two disjoint NX facet bodies. |
NXOpen.Facet.CurvatureBuilder |
Represents a NXOpen.Facet.CurvatureBuilder . |
NXOpen.Facet.DecimateFacetBodyBuilder |
Represents a NXOpen.Facet.DecimateFacetBodyBuilder . |
NXOpen.Facet.DetectPrimitivesBuilder |
This class manages the primitive shape detection for a facet body. |
NXOpen.Facet.ExtrudeFacetBodyBuilder |
Represents a NXOpen.Facet.ExtrudeFacetBodyBuilder It extrudes a NX Facet Body. |
NXOpen.Facet.ExtrudeProfileBuilder |
Represents a NXOpen.Facet.ExtrudeProfileBuilder It extrudes 3D closed profile between planes. |
NXOpen.Facet.FacetModelingCollection |
Collection of freeform facet operations. |
NXOpen.Facet.FacetedBody |
Represents a faceted body. |
NXOpen.Facet.FacetedBodyCollection |
Represents a collection of faceted bodies in a part |
NXOpen.Facet.FacetedEdge |
Represents a faceted edge. |
NXOpen.Facet.FacetedFace |
Represents a faceted face. |
NXOpen.Facet.FeatureExtractionBuilder |
Represents a NXOpen.Facet.FeatureExtractionBuilder It extracts feature lines or separates regions of different curvature from a facet body based on the curvature map. |
NXOpen.Facet.FillHoleBuilder |
This class finds and fills holes to a prescribed boundary smoothness condition |
NXOpen.Facet.MergeFacetBodyBuilder |
Represents a NXOpen.Facet.MergeFacetBodyBuilder It merges two overlapping NX facet bodies. |
NXOpen.Facet.MultiPatchAlignmentBuilder |
Aligns multiple facet bodies to one another without using reference points. |
NXOpen.Facet.PaintBrushBuilder |
This class manages the paint brush utility for a facet body. |
NXOpen.Facet.PaintFacetBodyBuilder |
This class manages the color painting on a facet body. |
NXOpen.Facet.STLImportBuilder |
The STL file import builder |
NXOpen.Facet.SelectFacetedBody |
Represents a single object selection. |
NXOpen.Facet.SelectFacetedBodyList |
Represents a list of objects on a selection list. |
NXOpen.Facet.SewFacetBodyBuilder |
Represents a NXOpen.Facet.SewFacetBodyBuilder It sews two touching NX facet bodies. |
NXOpen.Facet.SmoothFacetBodyBuilder |
Represents a NXOpen.Facet.SmoothFacetBodyBuilder . |
NXOpen.Facet.SnipFacetBodyBuilder |
Represents a SnipFacetBody builder |
NXOpen.Facet.SubdivideFacetBodyBuilder |
This class provides functionality to subdivide the polygons to increase the density of the facet bodies. |
Enumerations¶
BestFitAlignBuilderConstraintOptions Enumeration | Represents the constraint options |
BridgeFacetBodyBuilderInput Enumeration | Represents the option for keeping, deleting or hiding input two facet bodies after builder committing |
BridgeFacetBodyBuilderSmoothTypes Enumeration | Represents the smoothness type for the inserted new facets |
DecimateFacetBodyBuilderDecimateMethodType Enumeration | Decimate Method |
ExtrudeFacetBodyBuilderLimitType Enumeration | Represents the extrude limit type |
FacetedBodyFacetedbodyType Enumeration | Body type |
FacetedBodyCollectionType Enumeration | Specifies the type of facets created when copying or converting faceted bodies |
FacetedEdgeFacetededgeType Enumeration | Facet Edge type |
FacetedFaceFacetedfaceType Enumeration | Facet Face type |
FeatureExtractionBuilderInputActions Enumeration | Specifies how to handle the input facet bodies. |
FillHoleBuilderSmoothTypes Enumeration | Smoothness and boundary continuity options. |
FillHoleBuilderTargetTypes Enumeration | Options defining how to target holes for filling. |
FillHoleBuilderTypes Enumeration | Hole filling type options. |
MergeFacetBodyBuilderInput Enumeration | Represents the option for keeping, deleting or hiding input two facet bodies after builder committing |
MultiPatchAlignmentBuilderResolutionType Enumeration | Determines the number of facets used in the alignment. |
STLImportBuilderAngularToleranceTypes Enumeration | The angular tolerance types |
STLImportBuilderFacetBodyTypes Enumeration | These represent the type of body that will get created on importing the STL file |
STLImportBuilderSTLFileUnitsTypes Enumeration | The STL file units types |
SewFacetBodyBuilderInput Enumeration | Represents the option for keeping, deleting or hiding input two facet bodies after builder committing |
SewFacetBodyBuilderVertexIndex Enumeration | Index of the vertex |
SnipFacetBodyBuilderBoundaryFacetTreatmentMethod Enumeration | Boundary facet treatment type: |
SnipFacetBodyBuilderDirectionType Enumeration | Snipping direction when snipping type by profiles |
SnipFacetBodyBuilderTypes Enumeration | Snip method |
SubdivideFacetBodyBuilderInterpolationMethodType Enumeration | Subdivision interpolation methods |
SubdivideFacetBodyBuilderSubdivisionMethodType Enumeration | Subdivision methods |
Structs¶
FacetingParameters Struct | The structure of JA faceting parameters |