FacetedEdgeFacetededgeType Enumeration¶
NXOpen.Facet.FacetedEdge.FacetededgeType is an alias for NXOpen.Facet.FacetedEdgeFacetededgeType
-
class
NXOpen.Facet.
FacetedEdgeFacetededgeType
¶ Bases:
object
Facet Edge type
New in version NX8.5.1.
Enum Members
Enum Member Enum Member Description Undefined Linear Linear edgeCircular Circular edgeElliptical Elliptical edgeIntersection Intersection edgeSpline Spline edge-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-