BestFitAlignBuilderConstraintOptions Enumeration¶
NXOpen.Facet.BestFitAlignBuilder.ConstraintOptions is an alias for NXOpen.Facet.BestFitAlignBuilderConstraintOptions
-
class
NXOpen.Facet.
BestFitAlignBuilderConstraintOptions
¶ Bases:
object
Represents the constraint options
Enum Members
Enum Member Enum Member Description Free No constraintOnlyTranslation Only translationTranslationInPlane Translation in the planeTranslationAlongDirection Translation along directionOnlyRotation Only rotationRotationAroundPoint Rotation around specific pointRotationAroundLine Rotation around specific lineHoldToPlane Moving in the planeHoldToLine Moving along the line-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-