FillHoleBuilderSmoothTypes Enumeration¶
NXOpen.Facet.FillHoleBuilder.SmoothTypes is an alias for NXOpen.Facet.FillHoleBuilderSmoothTypes
-
class
NXOpen.Facet.
FillHoleBuilderSmoothTypes
¶ Bases:
object
Smoothness and boundary continuity options.
Enum Members
Enum Member Enum Member Description Linear Linear (triangulated) fill.Refined Smooth internal fill.TangentBased Smooth fill, boundary is based on facet body tangent.CurvatureBased Smooth fill, boundary is based on facet body curvature.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-