NumMU (material flow objects)
Syntax
<Path>.NumMU → integer |
The read-only attribute NumMu returns the number of MUs booked on the object designated by <Path>.
On length-oriented objects MUs may only be located on a part of the object. In this case they will only be counted if their booking point is actually located on the object.
Note:
When the object is not booked on another object either, Plant Simulation counts the MU as being part of the length-oriented object on which a part of the MU is located. This might, for example, occur, when an MU is moved from a Station onto a Conveyor.
Return Value
The return value has the data type integer.
Example
print ParallelStation.NumMU |
Related Topics
Tab Statistics of the material flow objects
Tab Statistics of the Container
Statistics Values of the Transporter
Related Topics
Miscellaneous Read-Only Attributes of the Material Flow ObjectsAssignedLockoutzones
Capacity (material flow object)
Class (read-only attribute)
Cont (material flow objects)
EntranceFree
EntranceOpen (material flow objects)
InternalClassName
IsSetUpFor
NumChildren
NumMUParts (material flow objects)
NumPartsSinceSetup
RemainingSetUpTime
RootFrame