EntranceOpen (material flow objects)
Syntax
<Path>.EntranceOpen → boolean |
The read-only attribute EntranceOpen returns if a mobile object can enter the material flow object because of current recovery or cycle times (true) or not (false).
Return Value
The return value has the data type boolean.
Example
print MyStation.EntranceOpen |
Related Topic
Related Topics
Miscellaneous Read-Only Attributes of the Material Flow ObjectsAssignedLockoutzones
Capacity (material flow object)
Class (read-only attribute)
Cont (material flow objects)
EntranceFree
InternalClassName
IsSetUpFor
NumChildren
NumMU (material flow objects)
NumMUParts (material flow objects)
NumPartsSinceSetup
RemainingSetUpTime
RootFrame