AssignedLockoutzones
Syntax
<Path>.AssignedLockoutzones → any |
The read-only attribute AssignedLockoutzones returns the LockoutZones assigned to the object designated by <Path>.
Return Value
The return value has the data type any.
Example
-- the station SP3 is assigned to one lockout zone |
-- the station SP5 is assigned to two lockout zones |
Related Topics
Related Topics
Miscellaneous Read-Only Attributes of the Material Flow ObjectsCapacity (material flow object)
Class (read-only attribute)
Cont (material flow objects)
EntranceFree
EntranceOpen (material flow objects)
InternalClassName
IsSetUpFor
NumChildren
NumMU (material flow objects)
NumMUParts (material flow objects)
NumPartsSinceSetup
RemainingSetUpTime
RootFrame