EntranceFree
Syntax
<Path>.EntranceFree → boolean |
The read-only attribute EntranceFree returns, if the entrance of the object designated by <Path> is not blocked (true), or if it is blocked (false). The entrance might be blocked because an MU is located there or because the capacity of the object is exhausted. The object may only receive an MU if the entrance is open and free.
Return Value
The return value has the data type boolean.
Example
if MyStation.EntranceFree AND |
Related Topic
Related Topics
Miscellaneous Read-Only Attributes of the Material Flow ObjectsAssignedLockoutzones
Capacity (material flow object)
Class (read-only attribute)
Cont (material flow objects)
EntranceOpen (material flow objects)
InternalClassName
IsSetUpFor
NumChildren
NumMU (material flow objects)
NumMUParts (material flow objects)
NumPartsSinceSetup
RemainingSetUpTime
RootFrame