NumMUParts (material flow objects)
Syntax
<Path>.NumMUParts → integer |
The read-only attribute NumMUParts returns the number of MUs located on the object designated by <Path> as a whole or in part.
Note that for length-oriented objects an MU may have exited the object with its front part while the rear is still located on the object. In this case NumMUParts counts both occupied lengths separately, although they form part of a single MU.
Note:
The read-only attribute NumMU returns the number of MUs whose booking point is located on the object. On point-oriented objects NumMUParts and NumMU always return the same value.
Return Value
The return value has the data type integer.
Example
if conveyor.NumMUParts 3 |
Related Topics
Related Topics
Miscellaneous Read-Only Attributes of the Material Flow ObjectsAssignedLockoutzones
Capacity (material flow object)
Class (read-only attribute)
Cont (material flow objects)
EntranceFree
EntranceOpen (material flow objects)
InternalClassName
IsSetUpFor
NumChildren
NumMU (material flow objects)
NumPartsSinceSetup
RemainingSetUpTime
RootFrame