Statistics Values (Transporter)
The tab Statistics shows the driving statistics of the Transporter.
Order occupied | Shows the time portion of its life-span during which the Transporter had an order and was loaded. | |
Order empty | Shows the time portion of its life-span during which the Transporter had an order and was not loaded ( Empty). | |
Home driving | Shows the time portion of its life-span during which the Transporter was returning to its base. | |
Ready | Shows the portion of the statistics collection period during which the Transporter was ready. | |
Failed | Shows the portion of the statistics collection period during which the Transporter was Failed. | |
Paused | Shows the portion of the statistics collection period during which the Transporter was Paused. | |
Unplanned | Shows the portion of the statistics collection period during which the Transporter was Unplanned,i.e., was not scheduled to work to the statistics collection period. | |
Empty | Shows the portion of the statistics collection period during which the Transporter was Empty. | |
Relative occupation | Shows the capacity-based ratio of the time during which the Transporter was occupied, not paused and not failed to the time the object was not paused and not failed. | |
Contents | Shows the number of MUs, which are located on the Transporter. | |
Minimum contents | Shows the minimum number of MUs, which were located on the Transporter. | |
Maximum contents | Shows the maximum number of MUs, which were located on the Transporter. | |
Entries | Shows the number of MUsthat entered the Transporter. When an MU enters the object, the object only counts the MU itself, not its contents: When a Transporter transporting several parts enters the object, the number of entries increases by 1, not by the number of parts located on the Transporter! | |
Exits | Shows the number of MUs that exited the Transporter. The rules described under Entries apply. | |
Traveled distance | Shows the distance which the Transporter traveled on a Track in meters. |
To view Driving Statistics of the Transporter in the Statistics Report, click the object in the Frame, and press F6 (Show Statistics Report), or click Show Statistics Report on the Home ribbon tab.