Empty
A material flow resource is empty, when no MU is booked on it and when the resource is not Failed, not Paused, or not Stopped. The empty time always is part of the Waiting time.
When the object has several processing stations, as for example the ParallelStation, you can query if an MU is located on a certain processing station. When the respective station is empty, the method returns true.
The Statistics Report shows the Empty Time below Resource Statistics of Stationary Resources.
SimTalk
Related Topics
Related Topics
Resource Statistics (material flow objects)Working (general description)
Setting-Up (general description)
Waiting (described)
Blocked
Powering up/down
Failed (resource statistics)
Stopped (material flow object, state)
Paused (material flow objects)
Unplanned (general description)
Relative Occupation