Copy Objects from Toolbar to Toolbar
To adapt simulation models that you created in previous versions of Plant Simulation, you can use the following technique to copy objects from one toolbar of the Toolbox to another. This is especially handy for Toolboxes that contain a large number of objects:
First, select the toolbar containing the object you would like to add to another tab.
Right-click the folder whose tab you would like to add the object to in the tree window and select Show Structure. This opens the window Structure. Expand the folder here.
Hold down the Ctrl key and click the object you would like to copy on its toolbar in the Toolbox. This selects the object in the tree window.
Drag the object from the tree window to the icon of the toolbar in the dialog Structure.
Go to Add Objects to the Toolbox or Delete Them from It