StatHomeDrivingPortion
Syntax
<MU-Path>.StatHomeDrivingPortion → real |
The read-only attribute StatHomeDrivingPortion returns the portion of its lifetime during which the Transporter designated by <MU-Path> was returning to its base.
Return Value
The return value has the data type real.
Example
print MyTrack.Transporter:1.StatHomeDrivingPortion |
Related Topics
Statistics Values of the Transporter
Statistics report, Statistics of the Transporters
Related Topics
Read-Only Attributes of the TransporterCollided
DistanceObjectBelowLimit
GetFrontWagon
GetRearWagon
GetTractor
HasRouteToDestination (Transporter)
StatBatChargeCount
StatBatChargePortion
StatHomeDrivingTime
StatOrderEmptyPortion
StatOrderEmptyTime
StatOrderOccPortion
StatOrderOccTime
StatTraveledDistance (Transporter)
StatTspFailCount
StatTspFailDelta
StatTspFailMu
StatTspFailPortion
StatTspFailTime
StatTspPausingCount
StatTspPausingDelta
StatTspPausingMu
StatTspPausingPortion
StatTspPausingTime
StatTspReadyCount
StatTspReadyDelta
StatTspReadyMu
StatTspReadyPortion
StatTspReadyTime
StatTspUnplannedCount
StatTspUnplannedDelta
StatTspUnplannedMu
StatTspUnplannedPortion
StatTspUnplannedTime