DistanceObjectBelowLimit
Syntax
<MU-Path>.DistanceObjectBelowLimit → object |
The read-only attribute DistanceObjectBelowLimit returns if the MU for which the distance of the Transporter designated by <MU-Path> is smaller than the value you set.
If the distance is not smaller than the defined value for any MU, DistanceObjectBelowLimit returns void.
Return Value
The return value has the data type object.
Example
var o : object := .MUs.Transporter:1.DistanceObjectBelowLimit |
print .UserObjects.MyTransporter1:10.DistanceObjectBelowLimit |
Related Topics
Related Topics
Read-Only Attributes of the TransporterCollided
GetFrontWagon
GetRearWagon
GetTractor
HasRouteToDestination (Transporter)
StatBatChargeCount
StatBatChargePortion
StatHomeDrivingPortion
StatHomeDrivingTime
StatOrderEmptyPortion
StatOrderEmptyTime
StatOrderOccPortion
StatOrderOccTime
StatTraveledDistance (Transporter)
StatTspFailCount
StatTspFailDelta
StatTspFailMu
StatTspFailPortion
StatTspFailTime
StatTspPausingCount
StatTspPausingDelta
StatTspPausingMu
StatTspPausingPortion
StatTspPausingTime
StatTspReadyCount
StatTspReadyDelta
StatTspReadyMu
StatTspReadyPortion
StatTspReadyTime
StatTspUnplannedCount
StatTspUnplannedDelta
StatTspUnplannedMu
StatTspUnplannedPortion
StatTspUnplannedTime