Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldJointBuilder.Types |
WeldJointBuilder.Types.CREATE_ATTRIBUTES
Create weld joints from attributed ship structures data.
|
static WeldJointBuilder.Types |
WeldJointBuilder.Types.CREATE_AUTOMATIC
Automatic weld joint creation.
|
static WeldJointBuilder.Types |
WeldJointBuilder.Types.CREATE_MANUAL
Manual weld joint creation.
|
static WeldJointBuilder.Types |
WeldJointBuilder.Types.CREATE_MULTIPLE
Create multiple weld joints from manual input.
|
Modifier and Type | Method and Description |
---|---|
WeldJointBuilder.Types |
WeldJointBuilder.createMethod()
Returns the creation method
License requirements: None. |
WeldJointBuilder.Types |
WeldJointBuilder.type()
Returns the creation type
License requirements: None. |
static WeldJointBuilder.Types |
WeldJointBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.Types |
WeldJointBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.Types[] |
WeldJointBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldJointBuilder.setCreateMethod(WeldJointBuilder.Types type)
License requirements: structure_weld ("STRUCTURE WELD") . |
void |
WeldJointBuilder.setType(WeldJointBuilder.Types type)
License requirements: structure_weld ("STRUCTURE WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.