public static class WeldJointBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CREATE_ATTRIBUTES
Create weld joints from attributed ship structures data.
|
static int |
_CREATE_AUTOMATIC
Automatic weld joint creation.
|
static int |
_CREATE_MANUAL
Manual weld joint creation.
|
static int |
_CREATE_MULTIPLE
Create multiple weld joints from manual input.
|
static WeldJointBuilder.Types |
CREATE_ATTRIBUTES
Create weld joints from attributed ship structures data.
|
static WeldJointBuilder.Types |
CREATE_AUTOMATIC
Automatic weld joint creation.
|
static WeldJointBuilder.Types |
CREATE_MANUAL
Manual weld joint creation.
|
static WeldJointBuilder.Types |
CREATE_MULTIPLE
Create multiple weld joints from manual input.
|
Modifier and Type | Method and Description |
---|---|
static WeldJointBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldJointBuilder.Types CREATE_AUTOMATIC
public static final WeldJointBuilder.Types CREATE_MANUAL
public static final WeldJointBuilder.Types CREATE_MULTIPLE
public static final WeldJointBuilder.Types CREATE_ATTRIBUTES
public static final int _CREATE_AUTOMATIC
public static final int _CREATE_MANUAL
public static final int _CREATE_MULTIPLE
public static final int _CREATE_ATTRIBUTES
public static WeldJointBuilder.Types valueOf(int value)
public static WeldJointBuilder.Types valueOf(String name)
public static WeldJointBuilder.Types[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.