Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.shipdesign |
Provides classes and interfaces for Ship Design.
|
Class and Description |
---|
ShipSession |
Class and Description |
---|
ApplicationUtils
Represents Generator which wrap the ship api for china
To obtain an instance of this class, refer to ShipSession Created in NX11.0.0 |
GeneralArrangementManager
Represents the interface for General Arrangement classes
To obtain an instance of this class, refer to ShipSession Created in NX12.0.0 |
Generator
Represents Generator which wrap the ship api for china
To obtain an instance of this class, refer to ShipSession Created in NX11.0.0 |
Generator.AskPlatesSpatialRelationsData
This class holds the data returned from
Generator.askPlatesSpatialRelations(nxopen.TaggedObject, nxopen.TaggedObject[], double) |
Generator.ClashType
Clash status to indicate to show space position relation between two bodies
1.Clashes in entities of the same dimension
Clash_interfere Two solid bodies interfere if they share a common volume
Two faces interfere if they share a common area, or they intersect.
|
Generator.ShipCustomerEnterApplication
Defines the callback function whenever an NX application is entered.
|
Generator.ShipCustomerExitApplication
Defines the callback function whenever an NX application is exited.
|
Navigator
Represents the interface for navigator action classes
Use the NavigatorCollection class to get a navigator Created in NX11.0.1 |
Navigator.NodeCheckCallback
Navigator node check callback.
|
Navigator.NodeContextMenuItemActionCallback
Navigator node context menu item callback.
|
Navigator.NodeContextMenuItemDefaultMenuItemCallback
Navigator node context menu item default callback.
|
Navigator.NodeContextMenuItemVisibilityCallback
Navigator node context menu item visibility callback.
|
Navigator.NodeDeselectedCallback
Navigator node deselected callback.
|
Navigator.NodesContextMenuItemActionCallback
Multiple navigator node context menu item callback.
|
Navigator.NodesContextMenuItemDefaultMenuItemCallback
Multiple navigator node context menu item default callback.
|
Navigator.NodesContextMenuItemVisibilityCallback
Multiple navigator node context menu item visibility callback.
|
Navigator.NodeSelectedCallback
Navigator node selected callback.
|
Navigator.ViewContextMenuItemActionCallback
Navigator view context menu item callback.
|
Navigator.ViewContextMenuItemVisibilityCallback
Navigator iew context menu item visibility callback.
|
NavigatorCollection
Represents the interface for navigator action classes
To obtain an instance of this class, refer to ShipSession Created in NX11.0.1 |
NavigatorNode
Represents the interface for navigator view classes
Use the NavigatorView class to create a navigator node Created in NX11.0.1 |
NavigatorView
Represents the interface for navigator view classes
Use the Navigator class to get a navigator view Created in NX11.0.0 |
ShipNavigatorNodeBuilder
Represents the ship navigator node builder to add or edit ship navigator node.
|
ShipNavigatorNodeBuilder.NodeTypes
Settings to indicate the type of ship navigator node.
|
ShipNavigatorRoot
Represents the interface for ship navigator root classes.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.