Interface | Description |
---|---|
ApplicationUtils |
Represents Generator which wrap the ship api for china
To obtain an instance of this class, refer to ShipSession Created in NX11.0.0 |
GeneralArrangementManager |
Represents the interface for General Arrangement classes
To obtain an instance of this class, refer to ShipSession Created in NX12.0.0 |
Generator |
Represents Generator which wrap the ship api for china
To obtain an instance of this class, refer to ShipSession Created in NX11.0.0 |
Generator.ShipCustomerEnterApplication |
Defines the callback function whenever an NX application is entered.
|
Generator.ShipCustomerExitApplication |
Defines the callback function whenever an NX application is exited.
|
Navigator |
Represents the interface for navigator action classes
Use the NavigatorCollection class to get a navigator Created in NX11.0.1 |
Navigator.NodeCheckCallback |
Navigator node check callback.
|
Navigator.NodeContextMenuItemActionCallback |
Navigator node context menu item callback.
|
Navigator.NodeContextMenuItemDefaultMenuItemCallback |
Navigator node context menu item default callback.
|
Navigator.NodeContextMenuItemVisibilityCallback |
Navigator node context menu item visibility callback.
|
Navigator.NodeDeselectedCallback |
Navigator node deselected callback.
|
Navigator.NodesContextMenuItemActionCallback |
Multiple navigator node context menu item callback.
|
Navigator.NodesContextMenuItemDefaultMenuItemCallback |
Multiple navigator node context menu item default callback.
|
Navigator.NodesContextMenuItemVisibilityCallback |
Multiple navigator node context menu item visibility callback.
|
Navigator.NodeSelectedCallback |
Navigator node selected callback.
|
Navigator.ViewContextMenuItemActionCallback |
Navigator view context menu item callback.
|
Navigator.ViewContextMenuItemVisibilityCallback |
Navigator iew context menu item visibility callback.
|
NavigatorCollection |
Represents the interface for navigator action classes
To obtain an instance of this class, refer to ShipSession Created in NX11.0.1 |
NavigatorNode |
Represents the interface for navigator view classes
Use the NavigatorView class to create a navigator node Created in NX11.0.1 |
NavigatorView |
Represents the interface for navigator view classes
Use the Navigator class to get a navigator view Created in NX11.0.0 |
ShipNavigatorNodeBuilder |
Represents the ship navigator node builder to add or edit ship navigator node.
|
ShipNavigatorRoot |
Represents the interface for ship navigator root classes.
|
ShipSession |
Class | Description |
---|---|
Generator.AskPlatesSpatialRelationsData |
This class holds the data returned from
Generator.askPlatesSpatialRelations(nxopen.TaggedObject, nxopen.TaggedObject[], double) |
Generator.ClashType |
Clash status to indicate to show space position relation between two bodies
1.Clashes in entities of the same dimension
Clash_interfere Two solid bodies interfere if they share a common volume
Two faces interfere if they share a common area, or they intersect.
|
ShipNavigatorNodeBuilder.NodeTypes |
Settings to indicate the type of ship navigator node.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.