Package | Description |
---|---|
nxopen.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static Generator.ClashType |
Generator.ClashType.ABUT_BIN_A
Bounding b topology abuts bounding a topology on the inside.
|
static Generator.ClashType |
Generator.ClashType.ABUT_BOUT_A
Bounding b topology abuts bounding a topology on the outside.
|
static Generator.ClashType |
Generator.ClashType.ABUT_NO_CLASS
Bounding topologies abut, in/outside unknown.
|
static Generator.ClashType |
Generator.ClashType.AIN_B
Body a is completly in body b, without abut.
|
static Generator.ClashType |
Generator.ClashType.BIN_A
Body b is completly in body a, without abut.
|
static Generator.ClashType |
Generator.ClashType.EXISTS
Clash exists; only this is requested.
|
static Generator.ClashType |
Generator.ClashType.INTERFERE
Bounding topologies interfere.
|
static Generator.ClashType |
Generator.ClashType.NONE
There is no clash between two bodies.
|
Modifier and Type | Method and Description |
---|---|
Generator.ClashType |
Generator.checkBodyClash(DisplayableObject bodyA,
DisplayableObject bodyB)
Check the clash between two bodys.
|
static Generator.ClashType |
Generator.ClashType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Generator.ClashType |
Generator.ClashType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Generator.ClashType[] |
Generator.ClashType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.