Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
PartVisualizationEmphasis.EdgesType |
PartVisualizationEmphasis.ShellOptions.edges
whether or not edges are displayed for de-emphasized
shaded geometry when the See-Thru style is set to Shell.
|
PartVisualizationEmphasis.EdgesType |
PartVisualizationEmphasis.OriginalColorShellOptions.edges
whether or not edges are displayed for de-emphasized shaded
geometry when the See-Thru style is set to Original Color
Shell.
|
PartVisualizationEmphasis.EdgesType |
PartVisualizationEmphasis.LayersOptions.edges
whether or not edges are displayed for de-emphasized
shaded geometry when the See-Thru style is set to Layers.
|
static PartVisualizationEmphasis.EdgesType |
PartVisualizationEmphasis.EdgesType.NORMAL
Displays edges for de-emphasized shaded geometry if
edges are normally displayed for shaded geometry.
|
static PartVisualizationEmphasis.EdgesType |
PartVisualizationEmphasis.EdgesType.OFF
Displays no edges for de-emphasized shaded geometry.
|
Modifier and Type | Method and Description |
---|---|
static PartVisualizationEmphasis.EdgesType |
PartVisualizationEmphasis.EdgesType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationEmphasis.EdgesType |
PartVisualizationEmphasis.EdgesType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationEmphasis.EdgesType[] |
PartVisualizationEmphasis.EdgesType.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
LayersOptions(NXColor.Rgb rgbInitial,
PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the LayersOptions object.
|
OriginalColorShellOptions(PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the OriginalColorShellOptions object.
|
ShellOptions(NXColor.Rgb rgbInitial,
PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the ShellOptions object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.