public static class PartVisualizationEmphasis.EdgesType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NORMAL
Displays edges for de-emphasized shaded geometry if
edges are normally displayed for shaded geometry.
|
static int |
_OFF
Displays no edges for de-emphasized shaded geometry.
|
static PartVisualizationEmphasis.EdgesType |
NORMAL
Displays edges for de-emphasized shaded geometry if
edges are normally displayed for shaded geometry.
|
static PartVisualizationEmphasis.EdgesType |
OFF
Displays no edges for de-emphasized shaded geometry.
|
Modifier and Type | Method and Description |
---|---|
static PartVisualizationEmphasis.EdgesType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationEmphasis.EdgesType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationEmphasis.EdgesType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartVisualizationEmphasis.EdgesType OFF
public static final PartVisualizationEmphasis.EdgesType NORMAL
public static final int _OFF
public static final int _NORMAL
public static PartVisualizationEmphasis.EdgesType valueOf(int value)
public static PartVisualizationEmphasis.EdgesType valueOf(String name)
public static PartVisualizationEmphasis.EdgesType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.