public static class PartVisualizationEmphasis.OriginalColorShellOptions extends Object implements Serializable
Modifier and Type | Field and Description |
---|---|
PartVisualizationEmphasis.EdgesType |
edges
whether or not edges are displayed for de-emphasized shaded
geometry when the See-Thru style is set to Original Color
Shell.
|
NXColor.Rgb |
edgesRgb
the color of edges displayed for de-emphasized shaded
geometry when the See-Thru style is set to Original Color
Shell.
|
int |
translucency
the translucency of de-emphasized shaded geometry when
the See-Thru style is set to Original Color Shell.
|
Constructor and Description |
---|
OriginalColorShellOptions() |
OriginalColorShellOptions(PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the OriginalColorShellOptions object.
|
public PartVisualizationEmphasis.EdgesType edges
public NXColor.Rgb edgesRgb
public int translucency
public OriginalColorShellOptions()
public OriginalColorShellOptions(PartVisualizationEmphasis.EdgesType edgesInitial, NXColor.Rgb edgesRgbInitial, int translucencyInitial)
edgesInitial
- whether or not edges are displayed for de-emphasized shaded
geometry when the See-Thru style is set to Original Color
Shell.edgesRgbInitial
- the color of edges displayed for de-emphasized shaded
geometry when the See-Thru style is set to Original Color
Shell.translucencyInitial
- the translucency of de-emphasized shaded geometry when
the See-Thru style is set to Original Color Shell. It is
a percentage value between 30 and 100.Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.