Package | Description |
---|---|
nxopen.mfg.mlp |
Provides classes and interfaces for Machining Line Planner.
|
Class and Description |
---|
Blank
Represents a Machining Line Planner blank
To obtain an instance of this class use GetBlankModel of Product. |
InProcessFeature
Represents a Machining Line Planner in-process feature
To obtain an instance of this class use GetInProcessFeatures of Operation or MachiningFeature. |
IProcess
Interface to the Machining Line Planner process
This is an abstract class, and cannot be instantiated. |
IResource
Interface to the Machining Line Planner resource
This is an abstract class, and cannot be instantiated. |
Line
Represents a Machining Line Planner line
To obtain an instance of this class use GetLine of ProcessPlan or ProcessSetup. |
MachiningFeature
Represents a Machining Line Planner machining feature
To obtain an instance of this class use GetMachiningFeature of InProcessFeature or GetMachiningFeatures of Workpiece or PartFeature. |
MachiningLinePlanner
Represents the Line Planner
Use the static method in this class to obtain an instance. |
Operation
Represents a Machining Line Planner operation
To obtain an instance of this class use GetOperation of InProcessFeature or GetOperations of ProcessSetup. |
Part
Represents a Machining Line Planner part
To obtain an instance of this class use GetPartModel of Product or PartFeature. |
PartFeature
Represents a Machining Line Planner part-feature
To obtain an instance of this class use GetPartFeature of MachiningFeature or GetPartFeatures or Part. |
ProcessPlan
Represents a Machining Line Planner process plan
To obtain an instance of this class use MachiningLinePlanner Created in NX11.0.1 |
ProcessSetup
Represents a Machining Line Planner process setup
To obtain an instance of this class use GetSetup of Operation, Workpiece or ToolSet or GetSetups on ProcessPlan or Line. |
Product
Represents a Machining Line Planner product
To obtain an instance of this class use GetProducts of ProcessPlan. |
ToolAssembly
Represents a Machining Line Planner tool assembly
To obtain an instance of this class use (not yet implemented!) |
ToolSet
Represents a Machining Line Planner tool set
To obtain an instance of this class use GetToolSet of ToolAssembly. |
Workpiece
Represents a Machining Line Planner workpiece
To obtain an instance of this class, use GetWorkpiece of MachiningFeature or GetWorkpieces of ProcessSetup or Product. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.