Package | Description |
---|---|
nxopen.mfg.mlp |
Provides classes and interfaces for Machining Line Planner.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Operation
Represents a Machining Line Planner operation
To obtain an instance of this class use GetOperation of InProcessFeature or GetOperations of ProcessSetup. |
interface |
ProcessSetup
Represents a Machining Line Planner process setup
To obtain an instance of this class use GetSetup of Operation, Workpiece or ToolSet or GetSetups on ProcessPlan or Line. |
Modifier and Type | Method and Description |
---|---|
IProcess[] |
IProcess.getConstraintPredecessors()
Get the Constraint Predecessors of this process (note that these are the immediate predecessors, this function does not recurse)
License requirements: None. |
IProcess[] |
IProcess.getConstraintSuccessors()
Get the Constraint Successors of this process (note that these are the immediate successors, this function does not recurse)
License requirements: None. |
IProcess[] |
IProcess.getPredecessors()
Get the Predecessors of this process (note that these are the immediate predecessors, this function does not recurse)
License requirements: None. |
IProcess[] |
IResource.getProcesses()
Get the Processes
License requirements: None. |
IProcess[] |
IProcess.getSuccessors()
Get the Successors of this process (note that these are the immediate successors, this function does not recurse)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.