Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static OrientBranchBuilder.BranchAngleMethod |
OrientBranchBuilder.BranchAngleMethod.ALIGN_AXIS_TO_VECTOR
method to rotate branch by an angle between two vectors
|
static OrientBranchBuilder.BranchAngleMethod |
OrientBranchBuilder.BranchAngleMethod.ANGLE
method to rotate branch by angle
|
static OrientBranchBuilder.BranchAngleMethod |
OrientBranchBuilder.BranchAngleMethod.ANGLEFROM_REFERENCE_VECTOR
method to rotate branch with respect to selected vectors
|
static OrientBranchBuilder.BranchAngleMethod |
OrientBranchBuilder.BranchAngleMethod.TWO_POINTS
method to rotate branch by and angle between two points
|
Modifier and Type | Method and Description |
---|---|
OrientBranchBuilder.BranchAngleMethod |
OrientBranchBuilder.branchAngleType()
Returns the user selected
OrientBranchBuilder.BranchAngleMethod
License requirements: routing_harness ("Routing Harness") Created in NX7.5.0 |
static OrientBranchBuilder.BranchAngleMethod |
OrientBranchBuilder.BranchAngleMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientBranchBuilder.BranchAngleMethod |
OrientBranchBuilder.BranchAngleMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientBranchBuilder.BranchAngleMethod[] |
OrientBranchBuilder.BranchAngleMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientBranchBuilder.setBranchAngleType(OrientBranchBuilder.BranchAngleMethod branchAngleType)
License requirements: routing_harness ("Routing Harness") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.